Write / Read
About Port Extensions

PortNADistanceUnit Property


Description

Sets and returns the units for specifying port extension delay in physical length (distance).

 VB Syntax

fixture.PortNADistanceUnit = value

Variable

(Type) - Description

fixture

A Fixturing Object

value

(enum naDistanceUnit) Choose from:

0 – naDistanceUnit_Meter

1 – naDistanceUnit_Feet

2 – naDistanceUnit_Inch

Return Type

Enum

Default

naDistanceUnit_Meter

Examples

fixture.PortNADistanceUnit(2)= naDistanceUnit_Meter 'Write

value = fixture.PortNADistanceUnit(2) 'Read

C++ Syntax

HRESULT get_PortNADistanceUnit(short portNum, tagNADistanceUnit*  *pVal);

HRESULT put_PortNADistanceUnit(short portNum, tagNADistanceUnit  newVal);

Interface

IFixturing4