Write/Read
About Fixturing

PortMatchingCktModel Property


Description

Sets and returns the Port Matching circuit model for the specified port number.

Note:  This command affects ALL measurements on the channel.

 VB Syntax

fixture.PortMatchingCktModel(port) = value

Variable

(Type) - Description

fixture

A Fixturing (object)

port

(Integer)  Port number to receive circuit model.

value

(Enum as  NAFixturingPortMatchCkt)  Circuit model. Choose from

0  naFixPMC_SLPC  Series L - Parallel C

1  naFixPMC_PCSL  Parallel C - Series L

2  naFixPMC_PLSC  Parallel L - Series C

3  naFixPMC_SCPL  Series C - Parallel L

4  naFixPMC_PLPC  Parallel L - Parallel C

5  naFixPMC_USER  Load S2P file  - also set filename to load with strPortMatch_S2PFile Property

6  naFixPMC_NONE  No circuit model

7  naFixPMC_SCPC  Series C - Parallel C

8  naFixPMC_PCSC  Parallel C - Series C

9  naFixPMC_SLPL  Series L - Parallel L

10  naFixPMC_PLSL  Parallel L - Series L

Return Type

Long Integer

Default

naFixPMC_NONE

Examples

fixture.PortMatchingCktModel(2) = naFixPMC_PLSC 'Write

value = fixture.PortMatchingCktModel(1) 'Read

C++ Syntax

HRESULT get_PortMatchingCktModel(short port tagNAFixturingPortMatchCkt *pVal)
HRESULT put_PortMatchingCktModel(short port  tagNAFixturingPortMatchCkt newVal)

Interface

IFixturing