Write / Read |
About Port Extensions |
Description |
Sets and returns the media type of the added fixture or transmission line. |
VB Syntax |
fixture.PortMedium (port)= value |
Variable |
(Type) - Description |
|
fixture |
A Fixturing Object |
|
port |
(Integer) Port Number for which media type is being set. |
|
value |
(enum NACalStandardMedium) - Medium of the transmission line of the standard. Choose from: 0 - naCoax - Coaxial Cable 1 - naWaveGuide - Waveguide |
Return Type |
Enum |
Default |
0 - naCoax |
Examples |
fixture.PortMedium(2)= naCoax 'Write value = fixture.PortMedium(2) 'Read |
C++ Syntax |
HRESULT get_PortMedium(short portNum, tagNACalStandardMedium* pVal); HRESULT put_PortMedium(short portNum, tagNACalStandardMedium newVal); |
Interface |
IFixturing4 |