Write/Read |
About Cal All |
Description |
Sets and returns the power level at which a Cal All calibration is to be performed. |
VB Syntax |
calAll.PowerLevel (port) = value |
Variable |
(Type) - Description |
calAll |
A CalibrateAllChannels (object) |
port |
(Long) Source port number. |
value |
(Double) Power level at which the calibration is to be performed. |
Return Type |
Double |
Default |
|
Examples |
calAll.PowerLevel = 0 'Power Level of cal value = calAll.PowerLevel 'returns the power level of the cal |
C++ Syntax |
HRESULT get_PowerLevel (long port, double val); HRESULT put_PowerLevel long port, double* newVal); |
Interface |
ICalibrateAllChannels |