Write/Read |
About Receiver Leveling |
Description |
Sets and returns the maximum power level for Safe Mode. |
VB Syntax |
RxLevel.PowerMax(srcPort) = value |
Variable |
(Type) - Description |
RxLevel |
A ReceiverLeveling Object |
srcPort |
(Long Integer) Source port for which to set the max power for Receiver Leveling. Note: If the source port is defined by a string name, such as an external source, a balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model, then use chan.getPortNumber to translate the string into a port number. To learn more see Remotely Specifying a Source Port |
value |
(Double) Maximum power level in dB. |
Return Type |
(Double) |
Default |
+ 30 |
Examples |
rxLevel.PowerMax (1) = 25 ' Write |
value = rxLevel.PowerMax 2' Read |
|
C++ Syntax |
HRESULT get_PowerMax(long port, double* pVal); HRESULT put_PowerMax(long port, double newVal); |
Interface |
IReceiverLevelingConfiguration |