Write/Read |
About Power Slope |
Description |
Turns point slope ON or OFF for all measurements on the channel. Use PowerSlope to set the slope value. |
VB Syntax |
chan.PowerSlopeState = state |
Variable |
(Type) - Description |
chan |
A Channel (object) |
state |
(boolean) False - Turns power slope OFF True - Turns point slope ON |
Return Type |
Boolean |
Default |
False |
Examples |
chan.PowerSlopeState = True 'Write |
state = chan.PowerSlopeState 'Read |
|
C++ Syntax |
HRESULT get_PowerSlopeState(VARIANT_BOOL *pVal) HRESULT put_PowerSlopeState(VARIANT_BOOL newVal) |
Interface |
IChannel18 |