Write/Read
About Guided Power Cal

PowerTableFilename Property


Description

Loads a file that defines a power table to be used during a SMC Guided Power Cal or Cal All Channels on a mmWave system. This feature is available because power sensors are NOT typically available at mmWave frequencies. Learn more.

 VB Syntax

guided.PowerTableFilename (n) = value

Variable

(Type) - Description

guided

A GuidedCalibration (object )

n

(Long)  Source port being calibrated.

value

(String) Full path and filename of a *.prn file that defines the power table. An error is returned if the file is not found.

Return Type

String

Default

Not applicable.

Examples

guided.PowerTableFilename(1) = "c:\powertable1.prn" 'Write

value = guided.PowerTableFilename(1) 'Read

C++ Syntax

HRESULT get_PowerTableFilename (long port, BSTR* val);

HRESULT put_PowerTableFilename (long port, BSTR newVal);

Interface

IGuidedCalibration9