Read-only
About Cal All

PropertyNamesByMeasurementClass Property


Description

Returns the list of valid property names by measurement class.

See a list of valid properties and values for each measurement class.

 VB Syntax

propNames = calAll.PropertyNamesByMeasurementClass (MeasurementClass)

Variable

(Type) - Description

propNames

(Variant Array) Variable to store the returned property names.

calAll

A CalibrateAllChannels (object)

MeasurementClass

(String) Measurement class name for which valid names are to be returned.

Return Type

Variant Array

Default

Not Applicable

Examples

props = calAll.PropertyNamesByMeasurementClass ("SMC")

C++ Syntax

HRESULT get_PropertyNamesByMeasurementClass(BSTR MeasurementClass, VARIANT* propNames);

Interface

CalibrateAllChannels