Write/Read |
About Pulse Measurements |
Description |
Sets the pulse measurement state for the channel. |
VB Syntax |
pulseMeas.PulseMeasMode = value |
Variable |
(Type) - Description |
pulseMeas |
A PulseMeasurementControl (object) |
value |
(Enum as NAPulseMeasurementMode) Choose from: (0) naPulseMeasurementOff - Turn OFF pulse measurements. (1) naPulseStandardMeasurement - Turn ON standard pulse measurements. (2) naPulseProfileMeasurement - Turn ON pulse profile measurements. |
Return Type |
Enum |
Default |
(0) naPulseMeasurementOff |
Examples |
pulse.PulseMeasMode = naPulseProfileMeasurement 'Write |
value = pulse.PulseMeasMode 'Read |
|
C++ Syntax |
HRESULT get_PulseMeasMode(tagNAPulseMeasurementMode* pVal); HRESULT put_PulseMeasMode(tagNAPulseMeasurementMode newVal); |
Interface |
IPulseMeasurementControl |