Write/Read |
About Pulse Measurements |
Description |
Sets and returns the stop time of the pulse. Pulse profile measurements provide a time domain (CW frequency) view of the pulse envelope. Profiling is performed using a measurement technique that "walks" a narrow receiver "snapshot" across the width of the pulse. This is analogous to using a camera to take many small snapshots of a wide image, then piecing them together to form a single, panoramic view. |
VB Syntax |
pulseMeas.PulseProfileStop = value |
Variable |
(Type) - Description |
|
pulseMeas |
A PulseMeasurementControl (object) |
|
value |
(double) - Stop time in seconds. Note: The stop value cannot be negative. |
Return Type |
Double |
Default |
N/A |
Examples |
pulseMeas.PulseProfileStop = 3e-3 'Write |
|
startprofile = pulseMeas.PulseProfileStop 'Read |
|
C++ Syntax |
HRESULT get_PulseProfileStop(double *pVal) |
Interface |
IPulseMeasControl3 |