Write/Read
About Phase Control

RatioedPowerCorrectionEnabled Property


Description

Write and read whether to use the ratioed power offset array. Use RatioedPowerCorrectionData Property to write or read the offset data.

 VB Syntax

phase.RatioedPowerCorrectionEnabled(srcPort) = value

Variable

(Type) - Description

phase

A PhaseControl Object

srcPort

(Long Integer) Source port for which to make phase control settings.

Note: If the source port is defined by a string name, such as an external source, a balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model, then use chan.getPortNumber to translate the string into a port number. To learn more see Remotely Specifying a Source Port

value

(Boolean) Ratioed power offset array state.

True – Apply offset array.

False – Do NOT apply offset array.

Return Type

Boolean

Default

False

Examples

phase.RatioedPowerCorrectionEnabled 1 = True ' Write

value = phase.RatioedPowerCorrectionEnabled 2' Read

C++ Syntax

HRESULT get_RatioedPowerCorrectionEnabled(long port, VARIANT_BOOL* pVal);

HRESULT put_RatioedPowerCorrectionEnabled(long port, VARIANT_BOOL newVal);

Interface

IPhaseControl