Write/Read
About Cal All

ReceiverAttenuator (Cal All) Property


Description

Sets and returns the Receiver Attenuator setting for a Cal All calibration.

 VB Syntax

calAll.ReceiverAttenuator (port) = value

Variable

(Type) - Description

calAll

A CalibrateAllChannels (object)

port

(Long) Receiver port number.

value

(Double) Attenuation value in dB for a Cal All calibration. Choose a valid value for the VNA model. See valid settings.

Return Type

Double

Default

0 (zero dB)

Examples

calAll.ReceiverAttenuator = 0 'Set value

value = calAll.ReceiverAttenuator 'Return value

C++ Syntax

HRESULT get_ReceiverAttenuator (long port, double val);

HRESULT put_ReceiverAttenuator long port, double* newVal);

Interface

ICalibrateAllChannels