Write/Read |
About Reference Level |
Description |
Sets or returns the value of the Y-axis Reference Level of the active trace. |
VB Syntax |
trce.ReferenceValue = value |
Variable |
(Type) - Description |
trce |
A Trace (object) |
value |
(double) - Reference Value. Units and range depend on the current data format. |
Return Type |
Double |
Default |
Not applicable |
Examples |
meas.ReferenceValue = 0 'Write |
rlev = meas.ReferenceValue 'Read |
|
C++ Syntax |
HRESULT get_ReferenceValue(double *pVal) |
Interface |
ITrace |