Write/Read
About Balanced Measurements

SSBMeasurement Property


Description

Sets and returns the measurement for the Single-Ended - Single-Ended - Balanced topology.

 VB Syntax

balMeas.SSBMeasurement = value

Variable

(Type) - Description

balMeas

A BalancedMeasurement (object)

value

(String) - Single-ended - Single-ended - Balanced Measurement parameter. Not case sensitive. Choose from:

 

Sss11

Sss12

Ssd13

Ssc13

Sss21

Sss22

Ssd23

Ssc23

Sds31

Sds32

Sdd33

Sdc33

Scs31

Scs32

Scd33

Scc33

Imb1

Imb2

CMRR1

(Sds31/Scs31)

CMRR2

(Sds32/Scs32)

Return Type

String

Default

Sss11

Examples

balMeas.SSBMeasurement = "Sss11" 'Write

variable = balMeas.SSBMeasurement  'Read

C++ Syntax

HRESULT get_SSBMeasurement(BSTR *pVal)

HRESULT put_SSBMeasurement(BSTR p newVal)

Interface

IBalancedMeasurement