Write/Read
About Scale Coupling

ScaleCouplingMethod Property


Description

Sets and returns the method of scale coupling.

 VB Syntax

win.ScaleCouplingMethod = value

Variable

(Type) - Description

win

An NAWindow (object)

Any window object can be used to set this global property.

value

(enum NAScaleCouplingMethod)

0 – naScaleCouplingOff - Scale Coupling is Off

1 – naScaleCouplingWindow - Traces within selected windows share scaling

2 – naScaleCouplingAll - Scaling is shared among traces in all selected windows

Select windows using ScaleCouplingState Property

Return Type

Enum

Default

0 – naScaleCouplingOff

Examples

win.ScaleCouplingMethod = naScaleCouplingWindow 'Write

method = app.ActiveNAWindow.ScaleCouplingMethod 'Read

C++ Syntax

HRESULT get_ScaleCouplingMethod(tagNAScaleCouplingMethod* couplingMethod);

HRESULT put_ScaleCouplingMethod(tagNAScaleCouplingMethod couplingMethod);

Interface

INAWindow2