Write/Read
About Mixer/Converter Settings

SegmentIsInputGreaterThanLO Property


Description

Set and read whether to use the Input frequency that is greater than the LO or less than the LO.

Send Apply before sending a query (read). Learn more.

 VB Syntax

conv.SegmentIsInputGreaterThanLO(index,range) = value

Variable

(Type) - Description

conv

A Converter Object

index

(Long integer) Segment which is being set. Choose a segment between 1 and the current segment count. Use SegmentCount Property to read the current count in the Applied Mixer.

range

(Enum as ConverterFrequencyRange) Range for which value is being set. Choose from:

0 - naInputFrequencies - set input power

1 - naOutputFrequencies - set output power

2 - naLO1Frequencies - set LO1 power

3 - naLO2Frequencies - set LO2 power

4 - naIFFrequencies - set IF power

value

(Boolean) -Choose from the following:

True - Use the Input that is Greater than the specified LO.

False - Use the Input that is Less than the specified LO.

Return Type

Boolean

Default

True

Examples

mxr.SegmentIsInputGreaterThanLO(1,2=1'sets segment 1, LO1 to Input greater

See example program

C++ Syntax

HRESULT get_SegmentIsInputGreaterThanLO(long index, tagConverterFrequencyRange range, VARIANT_BOOL *value);

HRESULT put_SegmentIsInputGreaterThanLO(long index, tagConverterFrequencyRange value, VARIANT_BOOL value);

Interface

IConverter5