Write/Read |
About Mixer/Converter Settings |
Description |
Set and read whether the mixing mode (high side or low side) for the mixer segment. Send Apply before sending a query (read). Learn more. |
VB Syntax |
conv.SegmentMixingMode(index,range) = value |
Variable |
(Type) - Description |
conv |
|
index |
(Long integer) Segment for which mixing mode being set. Choose a segment between 1 and the current segment count. Use SegmentCount Property to read the current count in the Applied Mixer. |
range |
(Enum as ConverterFrequencyRange) Range for which mixing mode is being set. Choose from: 1 - naOutputFrequencies - sets output frequencies for 1-stage or 2-stage mixers. 4 - naIFFrequencies - sets IF frequencies for the first LO in 2-stage mixers. |
value |
(Enum as ConverterSideBand) Choose from: 0 - naLowSide Input minus LO 1 - naHighSide Input plus LO |
Return Type |
Enum as ConverterSideBand |
Default |
0 - naLowSide |
Examples |
mxr.SegmentMixingMode(1,1)=1 'sets segment 1 output frequencies to Highside mixing. |
C++ Syntax |
HRESULT get_SegmentMixingMode(long index, tagConverterFrequencyRange range, tagConverterSideBand *value); HRESULT put_SegmentMixingMode(long index, tagConverterFrequencyRange value, tagConverterSideBand value); |
Interface |
IConverter5 |