Write/Read
About Mixer/Converter Settings

SegmentRangeMode Property


Description

Sets or returns the segment sweep mode (Swept or Fixed) for the specified range (Input/LO/Output).

Send Apply before sending a query (read). Learn more.

 VB Syntax

conv.SegmentRangeMode(index,range) = value

Variable

(Type) - Description

conv

A Converter Object

index

(Long integer) Segment for which mixing mode being set. Choose a segment between 1 and the current segment count. Use SegmentCount Property to read the current count in the Applied Mixer.

range

(Enum as ConverterFrequencyRange) Range for which sweep mode is being set. Choose from:

0 - naInputFrequencies - set input sweep mode.

1 - naOutputFrequencies - set output sweep mode.

2 - naLO1Frequencies - set LO1 sweep mode.

3 - naLO2Frequencies - set LO2 sweep mode.

4 - naIFFrequencies - set IF sweep mode.

value

(Enum as NARangeMode)  Choose from:

0 - naSwept  Range is swept

1 - naFixed  Range is fixed.

Return Type

Enum as NARangeMode

Default

Input and Output - naSwept

LO (1 and 2) - naFixed

Examples

mxr.SegmentRangeMode(1,1)=0 'sets segment 1 output range to swept.

See example program

C++ Syntax

HRESULT get_SegmentRangeMode(long index, tagConverterFrequencyRange range, tagNARangeMode *value);

HRESULT put_SegmentRangeMode(long index, tagConverterFrequencyRange value, tagNARangeMode value);

Interface

IConverter5