Write/Read
About Pulse Measurements

SoftwareGateState Property


Description

When set to OFF, the improved software gating sensitivity is turned OFF and all data outside the measurement band is zeroed.  This setting is used for troubleshooting purposes. There is NO user-interface control for this setting.

 VB Syntax

pulseMeas.SoftwareGateState = bool

Variable

(Type) - Description

pulseMeas

A PulseMeasurementControl (object)

bool

True - Turn ON software gating.

False - Turn OFF software gating.

Return Type

Boolean

Default

True

Examples

pulse.SoftwareGateState = True 'Write

value = pulse.SoftwareGateState 'Read

C++ Syntax

HRESULT get_SoftwareGateState(VARIANT_BOOL *pVal);

HRESULT put_SoftwareGateState(VARIANT_BOOL newVal);

Interface

IPulseMeasurementControl2