Write/Read |
About Ext Pulse Gens |
Description |
Sets and returns the source impedance of the pulse generator. |
VB Syntax |
extPulseGen.SourceImpedance = value |
Variable |
(Type) - Description |
extPulseGen |
An ExternalPulseGenerator (object) |
value |
(Double) Pulse generator source impedance. |
Return Type |
Double |
Default |
50 |
Examples |
extPulseGen.SourceImpedance = 50 'Write |
srcImp = extPulseGen.SourceImpedance 'Read |
|
C++ Syntax |
HRESULT get_SourceImpedance (double *pValue) HRESULT put_SourceImpedance (double newVal) |
Interface |
IExternalPulseGenerator |