Read-only
About Trace Statistics

StandardDeviation Property


Description

Returns the standard deviation of the measurement.
To retreive all 3 statistics value at the same time, use
meas.GetTraceStatistics

 VB Syntax

stdev = meas.StandardDeviation

Variable

(Type) - Description

stdev

(single) - Variable to store standard deviation value

meas

A Measurement (object)

Return Type

Single

Default

Not applicable

Examples

stdev = meas.StandardDeviation 'Read

C++ Syntax

HRESULT get_StandardDeviation(float* stdDeviation)

Interface

IMeasurement