Read-only
About Trace Statistics

GetTraceStatistics Method


Description

Returns all four Trace Statistics. To retreive individual Trace statistics, use Mean, PeakToPeak, StandardDeviation properties. Use ShowStatistics to display the statistics of the screen.

 VB Syntax

meas.GetTraceStatistics pp,mean,stdev

Variable

(Type) - Description

meas

A Measurement (object)

pp,mean,stdev

(double) - Dimensioned variables to store the returned values

Return Type

Double

Default

Not Applicable

Examples

'Dimension variables
Dim pp As Double
Dim mean As Double
Dim stdv As Double
meas.GetTraceStatistics pp, mean, stdv

C++ Syntax

HRESULT GetTraceStatistics(double* pp, double* mean, double* stdDeviation)

Interface

IMeasurement