Write/Read |
About Independent Power Calibration |
Description |
Sets and gets the start frequency for range <m> for source port<n>. |
VB Syntax |
PwrrCalRange.StartFrequency = freq |
Variable |
(Type) - Description |
freq |
(Long) - Variable to store the returned start frequency. |
PwrrCalRange |
A PowerCalRange (object) |
Return Type |
Double |
Default |
Not Applicable |
Example |
CalibrateAllChannels.IndependentPowerCalibration(3).PowerCalRange(1).StartFrequency = 20e9 'Write freq = CalibrateAllChannels.IndependentPowerCalibration(3).PowerCalRange(1).StartFrequency 'Read |
C++ Syntax |
HRESULT get_StartFrequency(double* freq); HRESULT put_StartFrequency(double freq); |
Interface |
IPowerCalRange |