Write/Read |
About DC Sources |
Description |
Sets and returns the ON / Off state of the specified DC source and port. |
VB Syntax |
dc.State(name,port) = state |
Variable |
(Type) - Description |
dc |
An DCStimulus (object) |
name,port |
(String) Name of the "DC source, port" Use Source Property to read a list of configured DC source names. To set the DC source to be always ON, do NOT specify a port. |
state |
Boolean. ON / Off state. Choose from: True - DC source/port enabled. False - DC source/port disabled. |
Return Type |
Boolean |
Default |
False |
Examples |
'Set AO1 to always ON dc.State "AO1",True 'Set MyDCSource to ON when the RF source for Port 1 is ON dc.State "MyDCSource,Port 1",ON 'Read state for MyDCSource,Port 1 dc.State? "MyDCSource,Port 1" |
C++ Syntax |
HRESULT get_State(BSTR name, VARIANT_BOOL * pValue); HRESULT put_State(BSTR name, VARIANT_BOOL newValue); |
Interface |
IDCStimulus |