| Write/Read | 
| Description | Turns the specified pulse generator ON and OFF. | 
| VB Syntax | pulse.State (n) = value | 
| Variable | (Type) - Description | 
| pulse | A PulseGenerator (object) | 
| n | (Integer) Pulse generator number. Choose from 0 to 4. Or use PulseGeneratorID to refer to an external pulse generator. 0 is the generator that pulses the ADC. | 
| value | True - turns pulse output ON. False - turns pulse output OFF. | 
| Return Type | Boolean | 
| Default | False | 
| Examples | pulse.State(1) = True 'Write | 
| value = pulse.State(4) 'Read | |
| C++ Syntax | HRESULT get_State(integer pulse, VARIANT_BOOL *pVal); HRESULT put_State(integer pulse, VARIANT_BOOL newVal); | 
| Interface | IPulseGenerator |