Read-only
About External Pulse Generators

PulseGeneratorID Property


Description

Returns the ID of the specified External Pulse Generator name. Use this ID number when setting properties on the PulseGenerator Object.

Use PulseGeneratorNames to read the names of the internal and configured external pulse generators.

 VB Syntax

value = chan.PulseGeneratorID (name)

Variable

(Type) - Description

value

(Long Integer) - Variable to store the returned ID.

chan

A Channel (object)

name

Name of the pulse generator. Use PulseGeneratorNames to read the names of configured pulse generators.

Return Type

Long Integer

Default

Not Applicable

Example

id = chan.PulseGeneratorID "My81110"

C++ Syntax

HRESULT get_PulseGeneratorID(long* count, BSTR name)

Interface

IChannel23