Write/Read
About Receiver Leveling

State (Rx Leveling) Property


Description

Sets and reads the state of Receiver Leveling for a specific source port.

 VB Syntax

RxLevel.State(srcPort) = value

Variable

(Type) - Description

RxLevel

A ReceiverLeveling Object

value

(Boolean) Choose from:

True - Receiver leveling ON

False - Receiver leveling OFF

srcPort

(Long Integer) Source port for which to set the state of Receiver Leveling.

Note: If the source port is defined by a string name, such as an external source, a balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model, then use chan.getPortNumber to translate the string into a port number. To learn more see Remotely Specifying a Source Port

Return Type

Variant Boolean

Default

False

Examples

rxLevel.State (1) = True ' Write

value = rxLevel.State 2' Read

C++ Syntax

HRESULT get_State(long port, VARIANT_BOOL* pLevelingState);

HRESULT put_State(long port, VARIANT_BOOL LevelingState);

Interface

IReceiverLevelingConfiguration