Read-only
About Embedded LO

StepData Property


Description

Returns an array of data from the specified tuning sweep.

 VB Syntax

value = embedLODiag.StepData (n)

Variable

(Type) - Description

value

(Variant Array) Variable to store the returned data.

embedLODiag

An EmbeddedLODiagnostic (object)

n

(Long) Tuning sweep number. Use NumberOfSweeps to find the number of sweeps taken.

Default

Not Applicable

Examples

data= embedLO.StepData 3 'read

C++ Syntax

HRESULT StepData(long sweep,VARIANT* pArray);

Interface

IEmbededLODiagnostic