Write/Read
About Active Match

SweepType Property


Description

Set and read the sweep type.

 VB Syntax

HotS22.SweepType = value

Variable

(Type) - Description

HotS22

A ActiveParametersApp (object)

value

(Enum as NAHOTSweepType) - Choose from:

  • 0 - naHOTS22LinearFrencySweep  Frequency linear sweep.

  • 1 - naHOTS22LogFrencySweep  Frequency log sweep.

  • 2 - naHOTS22PowerSweep  Power sweep.

  • 3 - naHOTS22MultiSweep  Multiple sweep. Sweeps frequency with fixed power and has several sweeps with different power values. This is called a 3D sweep: frequency, power, and phase.

Return Type

Enum

Default

0

Examples

HotS22.SweepType =  naHOTS22LinearFrencySweep 'Write

value = HotS22.SweepType 'Read

C++ Syntax

HRESULT get_SweepType(tagNAHOTSweepType* value)
HRESULT put_SweepType(tagNAHOTSweepType value)

Interface

IActiveChannelSettings