Write/Read
About Receiver Leveling

Tolerance Property


Description

Sets and returns the tolerance value for leveling sweeps.

 VB Syntax

RxLevel.Tolerance(srcPort) = value

Variable

(Type) - Description

RxLevel

A ReceiverLeveling Object

srcPort

(Long Integer) Source port for which to set the tolerance value for Receiver Leveling.

Note: If the source port is defined by a string name, such as an external source, a balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model, then use chan.getPortNumber to translate the string into a port number. To learn more see Remotely Specifying a Source Port

value

(Double) Tolerance level in dB.

Return Type

(Double)

Default

.1 dB

Examples

rxLevel.Tolerance (1) = .5 ' Write

value = rxLevel.Tolerance 2' Read

C++ Syntax

HRESULT get_Tolerance(long port, double* pVal);

HRESULT put_Tolerance(long port, double newVal);

Interface

IReceiverLevelingConfiguration