Write/Read
About Trace Max

TraceMax Property


Description

Maximizes (isolates) or restores the active trace in the active window. When TraceMax is ON, the active trace is the ONLY trace on the display. All other traces are hidden.

 VB Syntax

meas.TraceMax = state

Variable

(Type) - Description

meas

A Measurement (object)

state

(boolean) - Choose from:

True -  Maximizes / isolates the active trace in the window.

False - Restores other traces to be viewed in the window.

Return Type

Boolean

Default

False

Examples

meas.TraceMax = True

state = meas.TraceMax

C++ Syntax

HRESULT get_TraceMax(VARIANT_BOOL bState)
HRESULT put_TraceMax(VARIANT_BOOL* bState)

Interface

IMeasurement10