Write/Read |
About Cal All |
Description |
Sets and returns the prefix to be used when saving User Cal Sets that result from the Cal All session. The Meas Class and channel number are appended to this prefix for each calibrated channel. Use GeneratedCalsets to read the saved cal set names. If a Cal Set prefix is NOT set, the cal data for each channel will be saved only to cal registers. |
VB Syntax |
calAll.UserCalsetPrefix = prefix |
Variable |
(Type) - Description |
calAll |
A CalibrateAlChannels (object) |
prefix |
(String) User CalSet prefix. |
Return Type |
String |
Default |
Not Applicable |
Examples |
calAll.UserCalsetPrefix = "MyCalSet" 'Set csPrefix = calAll.UserCalsetPrefix 'Returns the CalSet prefix |
C++ Syntax |
HRESULT get_UserCalsetPrefix (BSTR calsetPrefix); HRESULT put_UserCalsetPrefix (BSTR* calsetPrefix); |
Interface |
ICalibrateAllChannels |