Write/Read |
About Vector Averaging |
Description |
Set and read the ON/OFF state of the vector averaging. |
VB Syntax |
sa.coherence.VectorAverageEnable = value |
Variable |
(Type) - Description |
sa.coherence |
A SpectrumAnalyzerCoherence (object) |
value |
(Boolean) Choose from: 0 - OFF - Vector averaging is set to OFF. 1 - ON - Vector averaging is set to ON. |
Return Type |
Boolean |
Default |
0 |
Examples |
sa.coherence.VectorAverageEnable = OFF Write |
value = sa.coherence.VectorAverageEnable 'Read |
|
C++ Syntax |
HRESULT put_VectorAverageEnable(VARIANT_BOOL bEnable); HRESULT get_VectorAverageEnable(VARIANT_BOOL* bEnable); |
Interface |
ICoherenceSA |