Read-only |
About IO Configuration |
Description |
Returns the valid resource string for the specified interface type. Use InterfaceTypes Property to read the valid interface types for the VNA. |
VB Syntax |
value = IOConfig.VisaResourceString (InterfaceType) |
Variable |
(Type) - Description |
value |
(String) variable to store the returned information. |
IOConfig |
An IOConfiguration object. |
InterfaceType |
(String) Name of Interface Type |
Return Type |
String |
Default |
Not Applicable |
Examples |
value = IOConfig.VisaResourceString "HISLIP" 'returns: TCPIP0::<compID>::hislip0::INST |
C++ Syntax |
HRESULT get VisaResourceString(BSTR interfaceType, long visaResourceID, BSTR* resourceString); |
Interface |
IIOConfiguration |