Write/Read
About External DC Devices

VoltageLimit Property


Description

Sets and returns the maximum output voltage value of the external DC Source. This command supports Keysight B2900A and N6700 series devices only.

 VB Syntax

extDC.VoltageLimit (devicename) = value

Variable

(Type) - Description

extDC

A ExternalDCDevice (object)

devicename

(String) Name of the device.

value

(Double) Voltage limit value.

Return Type

Double

Default

0

Examples

extDC.VoltageLimit("myDCDevice") = 4 'Write

limit = extDC.VoltageLimit("myDCDevice") 'Read

C++ Syntax

HRESULT get_VoltageLimit(BSTR devicename, double *vLimit)
HRESULT put_VoltageLimit(BSTR devicename, double newLimit)

Interface

IExternalDCDevice2