Read-only
About Embedded LO

XAxisStart Property


Description

Returns the X-Axis start value of the specified tuning sweep.

 VB Syntax

value = embedLODiag.XAxisStart (n)

Variable

(Type) - Description

value

(Double) Variable to store the returned data.

embedLODiag

An EmbeddedLODiagnostic (object)

n

(Long) Tuning sweep number. Use NumberOfSweeps to find the number of sweeps taken.

Default

Not Applicable

Examples

data= embedLO.XAxisStart 3 'read

C++ Syntax

HRESULT XAxisStart (long sweep, double* start);

Interface

IEmbededLODiagnostic