Read-only
About FOM

rangeNumber Property


Description

Returns the index number of the range within the FOM collection.

 VB Syntax

value = FOMRange.rangeNumber

Variable

(Type) - Description

value

(Long) - Variable to store the returned range number.

object

An FOMRange (object)

Return Type

Long

Default

Not Applicable

Examples

num = fomRange.rangeNumber 'Read

C++ Syntax

HRESULT get_rangeNumber(long  *pVal)

Interface

IFOMRange