Allows you to set the DIQ channel X-Axis domain and source.
| 
 
  | 
|
Click to view the command details.
See Also
| 
 Applicable Models: N522xB, N524xB (Write-only) Sets the information to display on the X-axis of the selected DIQ measurement. This command does not change the default setting for new traces.  | 
|||||||||||||
| 
 Parameters  | 
 
  | 
||||||||||||
| 
 <ch>  | 
 The Differential IQ channel number. If unspecified, value is set to 1.  | 
||||||||||||
| 
 <domain>  | 
 Character - Domain to display on the X-axis. Choose from: FREQuency - display the primary frequency range. POWer - display the power sweep range PHASe - display the phase sweep range DCValue - display the DC sweep range POINts - display the data points in the range  | 
||||||||||||
| 
 <source>  | 
 String - Specific source for the selected domain. Choose from the following: 
  | 
||||||||||||
| 
 Examples  | 
 CALC:DIQ:XAX FREQ,"F2" calculate:diq:xaxis power,"Port 1"  | 
||||||||||||
| 
 Query Syntax  | 
 Not Applicable  | 
||||||||||||
| 
 FREQ,"F1"  | 
|||||||||||||
| 
 Applicable Models: N522xB, N524xB (Read-only) Returns the X-Axis domain of the selected measurement.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <ch>  | 
 The Differential IQ channel number. If unspecified, value is set to 1.  | 
| 
 Example  | 
 CALC:DIQ:XAX:DOM? 'Possible returned values: FREQuency - display the primary frequency range. POWer - display the power sweep range PHASe - display the phase sweep range DCValue - display the DC sweep range POINts - display the data points in the range  | 
| 
 Return Type  | 
 Character  | 
| 
 FREQuency  | 
|
| 
 Applicable Models: N522xB, N524xB (Read-only) Returns the X-Axis source of the selected measurement.  | 
|
| 
 Parameters  | 
 
  | 
| 
 <ch>  | 
 The Differential IQ channel number. If unspecified, value is set to 1.  | 
| 
 Example  | 
 CALC:DIQ:XAX:SOURce? See CALC:DIQ:XAX for possible returned values.  | 
| 
 Return Type  | 
 String  | 
| 
 "F1"  | 
|