Calculate:FSimulator:Draft Commands

CALCulate:FSIMulator:DRAFt:

   | APPLy

| CIRCuit:

| ADD

| CATalog?

| DELete

| DEVice

| PORTs

| ARRay

| REVerse

| EMBED

| TYPE

| FILE

| EXTRapolate

| MODify

| NEXT?

| PARameter

| C

| C2

| DELay

| G

| G2

| L

| L2

| LOSS

| VALue

| R

| R2

| RIN

| ROUT

| Z0

| RESet

| STATe

| VNA

| PORTs

| DISCard

| EXTension:PORT:

    | DELay

    | DISTance

         | VALue

         | UNIT

    | END

    | LOSS

         | FREQuency

         | VALue

         | STATe

    | MEDium

    | WAVEguide

         | FCUToff

         | COUPle

    | VELocity

         | FACTor

         | COUPle

    | DCLoss:VALue

    | STATe

| SAVE

|SECTion

    | CIRCuit

| ENABle

| EXTension

| ENABle

      | ZCONversion

| ENABle

| ZCONversion

    | DIFFerential

         | STATe

         | BPORt
              | COMPLex

              | SCALar

         | :LPORt
              | COMPLex

              | SCALar

    | COMMonmode

         |  STATe

         |  BPORt
              | COMPLex

              | SCALar

         |  LPORt<pnum>
              | COMPLex

              | SCALar

    | SENDed:PORT

         |  STATe

         |  COMPLex

         | SCALar

   

 

See Also

 

Critical Note: CALCulate commands act on the selected measurement. You can select one measurement for each channel using Calc:Par:MNUM or Calc:Par:Select. Learn more.

CALCulate<cnum>:FSIMulator:DRAFt:APPLy

Applicable Models: All

(Write only) Copies the draft fixture to active fixture. Exact same functionality as CALC:FSIM:APPL

Parameters

Not applicable

Example

CALC:FSIM:DRAF:APPL

calculate:fsimulator:draft:apply

Return Type

Not applicable

Default

Not applicable


CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:ADD <block type>, <fixt port count>

Applicable Models: All

(Write only) Create a block of the specified block type with the specified fixture port count. By default, this block will be created on the VNA Port 1 with "de-embed".  It can be moved and changed to "embed" with commands below.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<circN>

Circuit Number

<block type>

FILe

SNP File Block (valid parameters: FILE, FILE:EXTRapolate)

RLGLoop

Ground Loop (Shunt L circuit model) (valid parameters:  R, L, C, G)

RCGLoop

Ground Loop (Shunt C circuit model) (valid parameters:  R, L, C, G)

CGGLoop

Ground Loop (Shunt C circuit model, but for convenience, user can specifier G instead of R) (valid parameters:  R, L, C, G)

FGLoop

Ground Loop (valid parameters:  FILE, FILE:EXTRapolate, file must be S1P file)

SLPC

Port Matching Circuit:  Series L - Shunt C (valid parameters:  R, R2, L, C,G, G2)

PCSL

Port Matching Circuit:  Shunt C - Series L (valid parameters:  R, R2, L, C, G, G2)

PLSC

Port Matching Circuit:  Shunt L - Series C (valid parameters:  R, R2, L, C, G, G2)

SCPL

Port Matching Circuit:  Series C - Shunt L (valid parameters:  R, R2, L, C, G, G2)

PLPC

Port Matching Circuit:  Shunt L - Shunt C (valid parameters:  R, R2, L, C, G, G2)

SCPC

Port Matching Circuit:  Series C - Shunt/ C (valid parameters:  R, R2, L, L2, C, C2, G, G2)

PCSC

Port Matching Circuit:  Shunt C - Series C (valid parameters:  R, R2, L, L2, C, C2, G, G2)

SLPL

Port Matching Circuit:  Series L - Shunt L (valid parameters:  R, R2, L, L2, C, C2, G, G2)

PLSL

Port Matching Circuit:  Shunt L - Series L (valid parameters:  R, R2, L, L2, C, C2, G, G2)

ILINe

Ideal Line. For this block type, user can specify delay and loss value.

TRANsformer

Transformer Circuit. For this block type, User can specify Rin and Rout values to represent a transformer.

D4PMatching

Differential Matching Circuit:  PLPC

D4PFile

Differential Matching Circuit:  File Type (S2P)

<fixt port count>

Number of port of block

Examples

CALC:FSIM:DRAF:CIRC:ADD SLPC,2

calculate2:fsimulator:draft:circuit:add SLPC,2

Query Syntax

Not Applicable

Return Type

Not Applicable

Default

Not Applicable


CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit:CATalog?

Applicable Models: All

(Read only) Returns a comma-separated list of circuit numbers created in the draft circuit.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

Examples

CALC:FSIM:DRAF:CIRC:CAT?

calculate2:fsimulator:draft:circuit:catalog?

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit:CATalog?

Return Type

comma-separated string

Default

Not Applicable


CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:DELete

Applicable Models: All

(Write only) Deletes the specified circuit.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<circN>

Circuit Number

Examples

CALC:FSIM:DRAF:CIRC:DEL

calculate2:fsimulator:draft:circuit:delete

Query Syntax

Not Applicable

Return Type

Not Applicable

Default

Not Applicable


CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:DEVice:PORTs[:ARRay] <port list - in, out>

Applicable Models: All

(Read-Write) Sets the Device ports for the specified circuit. The number of ports must be even and correspond to the number of ports of the fixture. This command can be used to reverse or change the order of ports in an SNP file.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<circN>

Circuit Number

Examples

CALC:FSIM:DRAF:CIRC:DEV:PORT 2,1

calculate2:fsimulator:draft:circuit:device:ports:array 2,1

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:DEVice:PORTs[:ARRay]?

Return Type

Numeric

Default

Not Applicable


CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:DEVice:PORTs:REVerse <bool>

Applicable Models: All

(Read-Write) Sets whether or not to reverse the ports on an existing S2P file.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<bool>

Choose from:

ON or 1 - Reverse the ports.

OFF or 0 - Do not reverse the ports.

<circN>

Circuit Number

Examples

CALC:FSIM:DRAF:CIRC:DEV:PORT:REV ON

calculate2:fsimulator:draft:circuit:device:ports:reverse 1

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:DEVice:PORTs:REVerse?

Return Type

Boolean

Default

0


CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:EMBED:TYPE <embed | deembed>

Applicable Models: All

(Read-Write) Sets whether the circuit should be embedded or de-embedded. Valid for all block Types.

The block is created using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<char>

Choose from :

EMBed - Add Network circuit.

DEEMbed - Remove Network circuit

<circN>

Circuit Number

Examples

CALC:FSIM:DRAF:CIRC:EMBED:TYPE EMBED

calculate2:fsimulator:draft:circuit:embed:type deembed

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:EMBED:TYPE?

Return Type

character

Default

EMBed


CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:FILE <filename>

Applicable Models: All

(Read-Write) Sets the filename. Valid blocks: FILe, D4PFile, FGLoop

The block is created using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<filename>

File name and extension (.s2P) of the de-embedding circuit.

Files are stored in the default folder "D:\".

To recall from a different folder, specify the full path name.

<circN>

Circuit Number

Examples

CALC:FSIM:DRAF:CIRC:FILE 'myFile.s2P'

calculate2:fsimulator:draft:circuit:file "D:\myFile.s2P"

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:FILE?

Return Type

string

Default

Not Applicable


CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:FILE:EXTRapolate <bool>

Applicable Models: All

(Read-Write) Sets whether or not extrapolation is allowed. Valid blocks: FILe, D4PFile, FGLoop.

The block is created using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<bool>

Choose from:

ON or 1 - Turns Extrapolation ON

OFF or 0 - Turns Extrapolation OFF

<circN>

Circuit Number

Examples

CALC:FSIM:DRAF:CIRC:FILE:EXTR ON

calculate2:fsimulator:draft:circuit:file:extrapolate 1

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:FILE:EXTRapolate?

Return Type

Boolean

Default

OFF


CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:FILE:MODify <enum>

Applicable Models: All

(Read-Write) Sets all reflection and crosstalk parameters on the DUT side to zero. Learn more.

The block is created using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<enum>

Choose from:

NONE - Does not modify the block.

NREFlect - Sets all reflection parameters on the DUT-side to zero.

NXTalk - Sets all reflection and crosstalk parameters on the DUT-side to zero.

<circN>

Circuit Number

Examples

CALC:FSIM:DRAF:CIRC:FILE:MOD NONE

calculate2:fsimulator:draft:circuit:file:modify nreflect

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:FILE:MODify?

Return Type

Enumeration

Default

NONE


CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:NEXT?

Applicable Models: All

(Read only) Returns the next free circuit number than be used to create a new circuit block

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<circN>

Circuit Number

Examples

CALC:FSIM:DRAF:CIRC:NEXT?

calculate2:fsimulator:draft:circuit:next?

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit:NEXT?

Return Type

Numeric

Default

Not Applicable


CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:C <value>

Applicable Models: All

(Read-Write) Sets the capacitance (C) circuit element for the specified circuit. Valid blocks: RLGLoop, RCGLoop, CGGLoop, SLPC, PCSL, PLSC, SCPL, PLPC, SCPC, PCSC, SLPL, PLSL.

The block is created using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<value>

Capacitance value in farads. Choose a value between -1E18 to 1E18

<circN>

Circuit Number

Examples

CALC:FSIM:DRAF:CIRC:PAR:C 0.00002

calculate2:fsimulator:draft:circuit:parameter:C 0.00002

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:C?

Return Type

Numeric

Default

0


CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:C2 <value>

Applicable Models: All

(Read-Write) Sets the capacitance (C2) circuit element for the specified circuit. Valid blocks: SLPC, PCSL, PLSC, SCPL, PLPC, SCPC, PCSC, SLPL, PLSL

The block is create using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<value>

Capacitance value in farads. Choose a value between -1E18 to 1E18

<circN>

Circuit Number

Examples

CALC:FSIM:DRAF:CIRC:PAR:C2 0.00002

calculate2:fsimulator:draft:circuit:parameter:C2 0.00002

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:C2?

Return Type

Numeric

Default

0


CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:DELay <num>

Applicable Models: All

(Read-Write) Sets port extension delay in time. Valid blocks: ILIN.

The block is create using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<num>

The port extension in seconds; may include suffix. Choose a number between: -1E18 and 1E18

<circN>

Circuit Number

Examples

CALC:FSIM:DRAF:CIRC:PAR:DEL 2MS

calculate2:fsimulator:draft:circuit:parameter:delay .00025

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:DEL?

Return Type

Numeric

Default

0


CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:G <value>

Applicable Models: All

(Read-Write) Sets the conductance (G) circuit element for the specified circuit. Valid blocks: RLGLoop, RCGLoop, CGGLoop, SLPC, PCSL, PLSC, SCPL, PLPC, SCPC, PCSC, SLPL, PLSL.

The block is create using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<value>

Conductance value in siemens. Choose a value between -1E18 to 1E18

<circN>

Circuit Number

Examples

CALC:FSIM:DRAF:CIRC:PAR:G 0.00002

calculate2:fsimulator:draft:circuit:parameter:g 0.00002

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:G?

Return Type

Numeric

Default

0


CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:G2 <value>

Applicable Models: All

(Read-Write) Sets the conductance (G2) circuit element for the specified circuit. Valid blocks: SLPC, PCSL, PLSC, SCPL, PLPC, SCPC, PCSC, SLPL, PLSL

The block is create using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<value>

Conductance value in siemens. Choose a value between -1E18 to 1E18

<circN>

Circuit Number

Examples

CALC:FSIM:DRAF:CIRC:PAR:G2 0.00002

calculate2:fsimulator:draft:circuit:parameter:g2 0.00002

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:G2?

Return Type

Numeric

Default

0


CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:L <value>

Applicable Models: All

(Read-Write) Sets the inductance (L) circuit element for the specified circuit. Valid blocks: RLGLoop, RCGLoop, CGGLoop, SLPC, PCSL, PLSC, SCPL, PLPC, SCPC, PCSC, SLPL, PLSL.

The block is create using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<value>

Inductance value in henries. Choose a value between -1E18 to 1E18

<circN>

Circuit Number

Examples

CALC:FSIM:DRAF:CIRC:PAR:L 0.00002

calculate2:fsimulator:draft:circuit:parameter:l 0.00002

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:L?

Return Type

Numeric

Default

0


CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:L2 <value>

Applicable Models: All

(Read-Write) Sets the inductance (L2) circuit element for the specified circuit. Valid blocks: SLPC, PCSL, PLSC, SCPL, PLPC, SCPC, PCSC, SLPL, PLSL

The block is create using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<value>

Inductance value in henries. Choose a value between -1E18 to 1E18

<circN>

Circuit Number

Examples

CALC:FSIM:DRAF:CIRC:PAR:L2 0.00002

calculate2:fsimulator:draft:circuit:parameter:l2 0.00002

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:L2?

Return Type

Numeric

Default

0


CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:LOSS:VALue <num>

Applicable Models: All

(Read-Write) Sets the loss at DC. Valid blocks: ILIN.

The block is create using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<num>

Loss in dB. Choose a value between -90 and 90.

<circN>

Circuit Number

Examples

CALC:FSIM:DRAF:CIRC:PAR:LOSS:VAL 1.5

calculate2:fsimulator:draft:circuit:parameter:loss:value .1

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:LOSS:VALue?

Return Type

Numeric

Default

0


CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:R <value>

Applicable Models: All

(Read-Write) Sets the resistance (R) circuit element for the specified circuit. Valid blocks: RLGLoop, RCGLoop, CGGLoop, SLPC, PCSL, PLSC, SCPL, PLPC, SCPC, PCSC, SLPL, PLSL.

The block is create using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<value>

Resistance value in ohms. Choose a value between -1E18 to 1E18

<circN>

Circuit Number

Examples

CALC:FSIM:DRAF:CIRC:PAR:R 0.00002

calculate2:fsimulator:draft:circuit:parameter:r 0.00002

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:R?

Return Type

Numeric

Default

0


CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:R2 <value>

Applicable Models: All

(Read-Write) Sets the resistance (R2) circuit element for the specified circuit. Valid blocks: SLPC, PCSL, PLSC, SCPL, PLPC, SCPC, PCSC, SLPL, PLSL

The block is create using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<value>

Resistance value in ohms. Choose a value between -1E18 to 1E18

<circN>

Circuit Number

Examples

CALC:FSIM:DRAF:CIRC:PAR:R2 0.00002

calculate2:fsimulator:draft:circuit2:parameter:r2 0.00002

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:R2?

Return Type

Numeric

Default

0


CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:RIN <value>

Applicable Models: All

(Read-Write) Sets the resistance (R) value at input of transformer (real only). Valid blocks: TRANs

The block is create using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<value>

Resistance value in ohms. Choose a value between -1E18 to 1E18

<circN>

Circuit Number

Examples

CALC:FSIM:DRAF:CIRC:PAR:RIN 0.00002

calculate2:fsimulator:draft:circuit2:parameter:rin 0.00002

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:RIN?

Return Type

Numeric

Default

0


CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:ROUT <value>

Applicable Models: All

(Read-Write) Sets the resistance (R) value at output of transformer (real only). Valid blocks: TRANs

The block is create using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<value>

Resistance value in ohms. Choose a value between -1E18 to 1E18

<circN>

Circuit Number

Examples

CALC:FSIM:DRAF:CIRC:PAR:ROUT 0.00002

calculate2:fsimulator:draft:circuit2:parameter:rout 0.00002

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:ROUT?

Return Type

Numeric

Default

0


CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:Z0 <value>

Applicable Models: All

(Read-Write) Sets the impedance (Z0) for the ideal block (scalar value). Valid blocks: ILIN.

The block is create using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<value>

Impedance value in ohms. Choose a value between -1E18 to 1E18

<circN>

Circuit Number

Examples

CALC:FSIM:DRAF:CIRC:PAR:Z0 0.00002

calculate2:fsimulator:draft:circuit:parameter:z0 0.00002

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:PARameter:Z0?

Return Type

Numeric

Default

50


CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit:RESet

Applicable Models: All

(Write only) Resets the circuit section to preset values

Note:  This command impacts the circuits and the port extensions.  It does not change any impedance conversion values.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

Examples

CALC:FSIM:DRAF:CIRC:RES

calculate2:fsimulator:draft:circuit:reset

Query Syntax

Not Applicable

Return Type

Not Applicable

Default

Not Applicable


CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:STATe <bool>

Applicable Models: All

(Read-Write) Turns the circuit ON and OFF. Valid for all block types

The block is create using CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:ADD <block type>, <fixt port count>. Setting a value not used by the selected circuit will have no affect. Learn more.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<bool>

Choose from:

ON or 1 - Turns the circuit ON

OFF or 0 - Turns the circuit OFF

<circN>

Circuit Number

Examples

CALC:FSIM:DRAF:CIRC:STAT ON

calculate2:fsimulator:draft:circuit1:state off

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:STATe?

Return Type

Boolean

Default

ON


CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit<circN>:VNA:PORTs <port list>

Applicable Models: All

(Read-Write) Sets the VNA ports for the specified circuit.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<circN>

Circuit Number

Examples

CALC:FSIM:DRAF:CIRC:VNA:PORT 2

calculate2:fsimulator:draft:circuit2:vna:ports 2

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:CIRCuit[n]:VNA:PORTs?

Return Type

Numeric

Default

Not Applicable


CALCulate<cnum>:FSIMulator:DRAFt:DISCard

Applicable Models: All

(Write only) Copies the active fixture into scratch/draft fixture (discards changes on scratch/draft fixture)

Parameters

Not applicable

Example

CALC:FSIM:DRAF:DISC

calculate:fsimulator:draft:discard

Return Type

Not applicable

Default

Not applicable


CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:DELay <value>

Applicable Models: All

(Read-Write) Sets and returns the delay value in time at the specified port.

Note:  This command affects ALL measurements on the specified channel.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1.

<pnum>

Port Number that will receive the delay setting. If unspecified, value is set to 1.

<value>

The port extension in seconds; may include suffix. Choose a number between: -1E18 and 1E18e.

Examples

CALC:FSIM:DRAF:EXT:PORT1:DEL 0.02
calculate:fsimulator:draft:extension:port2:delay .003

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:DELay?

Return Type

Numeric

Default

0


CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:DISTance:UNIT <char>

Applicable Models: All

(Read-Write) Sets and returns the units for specifying port extension delay in physical length (distance).

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1.

<pnum>

Port Number. This number is ignored and all ports have the same setting.

<char>

Units for delay in distance. Choose from:

  • METer

  • FEET

  • INCH

Examples

CALC:FSIM:DRAF:EXT:PORT2:DIST:UNIT MET
calculate:fsimulator:draft:extension:port3:distance:unit inch

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT:DISTance:UNIT?

Return Type

Character

Default

METer


CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:DISTance:VALue <value>

Applicable Models: All

(Read-Write) Sets and returns the port extension delay in physical length (distance).

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1.

<pnum>

Port Number that will receive the delay setting. If unspecified, value is set to 1.

<value>

Physical length of fixture of added transmission line. First specify units with :CALC:FSIM:DRAF:EXT:PORT:DIST:UNIT

Examples

CALC:FSIM:DRAF:EXT:PORT1:DIST:VAL 12
calculate:fsimulator:draft:extension:port2:distance:value .003

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:DISTance:VALue?

Return Type

Numeric

Default

0


CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:END

Applicable Models: All

(Write Only) Moves the port extension block to the left-most side of the circuit sections. This command allows the port extensions to be moved around in the circuit . This command should be executed after adding the other block. Because adding the block resets the port extension block position.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1.

<pnum>

Port Number that will receive the delay setting. If unspecified, value is set to 1.

Examples

CALC:FSIM:DRAF:EXT:PORT1:END
calculate:fsimulator:draft:extension:port2:end

Query Syntax

Not applicable

Return Type

Not applicable

Default

Not applicable


CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:LOSS<n>:FREQuency <value>

Applicable Models: All

(Read-Write) Sets and returns the frequency for the Freq and Loss pair number and for the specified port number.

Learn about Loss Compensation values.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<pnum>

Port Number that will receive the freq/loss settings. If unspecified, value is set to 1.

<n>

Freq and Loss pair number. Choose from 1 or 2.  If unspecified, value is set to 1.

<value>

Frequency value. Choose a frequency within the frequency span of the VNA.

Examples

CALC:FSIM:DRAF:EXT:PORT1:LOSS2:FREQ 10E9
calculate:fsimulator:draft:extension:port2:loss1:frequency 2E10

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:LOSS<n>:FREQuency?

Return Type

Numeric

Default

0


CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:LOSS<n>:VALue <value>

Applicable Models: All

(Read-Write) Sets and returns the Loss value for the specified port number.

Learn about Loss Compensation values.

Note:  This command affects ALL measurements on the specified channel.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<pnum>

Port Number that will receive the Freq/Loss settings. If unspecified, value is set to 1.

<n>

Loss "Use" number. Choose from 1 or 2. If unspecified, value is set to 1.

<value>

Loss in dB. Choose a value between -90 and 90

Examples

CALC:FSIM:DRAF:EXT:PORT:LOSS1:VAL 1

calculate:fsimulator:draft:extension:port2:loss2:value .1

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:LOSS<n>:VALue?

Return Type

Numeric

Default

0


CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:LOSS<n>[:STATe] <bool>

Applicable Models: All

(Read-Write) Sets and returns the ON/OFF state for the Freq and Loss pair number and for the specified port number.

Learn about Loss Compensation values.

Note:  This command affects ALL measurements on the specified channel.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<pnum>

Port Number that will receive the Freq/Loss settings. If unspecified, value is set to 1.

<n>

Freq and Loss pair. Choose from 1 or 2. If unspecified, value is set to 1.

<value>

State of Freq and Loss values for port extension.

0 or OFF  Specified Freq and Loss values are OFF

1 or ON  Specified Freq and Loss values are ON

Examples

CALC:FSIM:DRAF:EXT:PORT:LOSS:STAT 0
calculate:fsimulator:draft:extension:port2:loss2:state on

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:LOSS<n>:STATe?

Return Type

Boolean

Default

OFF


CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:DCLoss:VALue <value>

Applicable Models: All

(Read-Write) Sets and returns the Port Loss at DC value for the specified port number.

Learn about Loss Compensation values.

Note:  This command affects ALL measurements on the specified channel.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<pnum>

Port number to receive Loss value. If unspecified, value is set to 1.

<value>

Loss in dB. Choose a value between -90 and 90

Examples

CALC:FSIM:DRAF:EXT:PORT:DCL:VAL 1.5

calculate:fsimulator:draft:extension:port2:dcloss:value .1

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:DCLoss:VALue?

Return Type

Numeric

Default

0


CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:MEDium <char>

Applicable Models: All

(Read-Write) Sets and returns the media type of the added fixture or transmission line.

See also SENS:CORR:EXT:PORT:SYSMedia

Note:  This command affects ALL measurements on the specified channel.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<pnum>

Port Number. This number is ignored and all ports have the same setting.

<char>

Medium type. Choose from:

  • COAX

  • WAVEguide

Examples

CALC:FSIM:DRAF:EXT:PORT:MED COAX

calculate:fsimulator:draft:extension:port2:medium waveguide

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:MEDium?

Return Type

Character

Default

COAX


CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:WAVEguide:FCUToff <value>

Applicable Models: All

(Read-Write) Sets and returns the cuttoff (minimum) frequency of the added waveguide fixture or transmission line.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<pnum>

Port Number for which media type is being set. If unspecified, value is set to 1.

<value>

Cutoff frequency in Hz.

This value is ignored when CALC:FSIM:DRAF:EXT:PORT:MED is set to COAX for the same port.

Examples

CALC:FSIM:DRAF:EXT:PORT:WAVE:FCUT 1e8

calculate:fsimulator:draft:extension:port2:waveguide:cutoff 100Mhz

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:WAVEguide:FCUToff?

Return Type

Numeric

Default

System Media Cutoff Frequency


CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:WAVEguide:COUPle <bool>

Applicable Models: All

(Read-Write) Sets and returns the state of coupling with the system Velocity Factor value. Learn more.

Note:  This command potentially affects ALL measurements on the VNA.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<pnum>

Port Number. This number is ignored and all ports have the same setting.

<bool>

Coupling state. Choose from:

  • ON (or 1) - Velocity Factor is coupled with the system setting.

  • OFF (or 0) - Velocity Factor is NOT coupled with the system setting.

Examples

CALC:FSIM:DRAF:EXT:PORT:WAVE:COUP 1

calculate:fsimulator:draft:extension:port2:waveguide:couple off

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:WAVEguide:COUPle?

Return Type

Boolean

Default

1 or ON (Coupled)


CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:VELocity:FACtor <value>

Applicable Models: All

(Read-Write) Sets and returns the velocity factor of the fixture or added transmission line.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<pnum>

Port Number for which velocity factor is being set. If unspecified, value is set to 1.

<value>

Velocity Factor.

Set SENS:CORR:EXT:PORT:SYSV to use the system velocity factor.

Examples

CALC:FSIM:DRAF:EXT:PORT:VEL:FAC .6

calculate:fsimulator:draft:extension:port2:velocity:factor 1

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:VELocity:FACtor?

Return Type

Numeric

Default

System Velocity Factor


CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:VELocity:COUPle <bool>

Applicable Models: All

(Read-Write) Sets and returns the state of coupling with the system Velocity Factor value. Learn more.

Note:  This command potentially affects ALL measurements on the VNA.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<pnum>

Port Number. This number is ignored and all ports have the same setting.

<bool>

Coupling state. Choose from:

  • ON (or 1) - Velocity Factor is coupled with the system setting.

  • OFF (or 0) - Velocity Factor is NOT coupled with the system setting.

Examples

CALC:FSIM:DRAF:EXT:PORT:VEL:COUP 1

calculate:fsimulator:draft:extension:port2:velocity:couple off

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>:VELocity:COUPle?

Return Type

Boolean

Default

1 or ON (Coupled)


CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>[:STATe] <bool>

Applicable Models: All

(Read-Write) Sets and returns the state of port extension for the specified port.

Note:  This command potentially affects ALL measurements on the VNA.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<pnum>

Port Number for which port extension is being set. If unspecified, value is set to 1.

<bool>

Port extension state. Choose from:

  • ON (or 1) - Port extension is on

  • OFF (or 0) - Port extension is off.

Examples

CALC:FSIM:DRAF:EXT:PORT:STAT 1

calculate:fsimulator:draft:extension:port2:state off

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:EXTension:PORT<pnum>[:STATe]?

Return Type

Boolean

Default

0


CALCulate<cnum>:FSIMulator:DRAFt:SAVE <snpName>

Applicable Models: All

(Write only) Saves SNP file corresponding to the entire scratch/draft fixture.

Parameters

 

<snpName>

String - snp file name. Appends ".sNp" depending on num ports

Example

CALC:FSIM:DRAF:SAVE "myFixure"

calculate:fsimulator:draft:save "D:\myfixture"

Return Type

Not applicable

Default

Not applicable


CALCulate<cnum>:FSIMulator:DRAFt:SECTion:CIRCuit:ENABle <ON | OFF>

Applicable Models: All

(Read-Write) Turns all circuits ON or OFF for all ports.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<ON | OFFl>

ON (or 1) - turns all circuits ON.

OFF (or 0) -turns all circuits OFF.

Examples

CALC:FSIM:DRAF:SECT:CIRC:ENAB ON

calculate2:fsimulator:draft:section:circuit:enable off

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:SECTionCIRCuit:ENABle?

Return Type

Boolean (1 = ON, 0 = OFF)

Default

ON


CALCulate<cnum>:FSIMulator:DRAFt:SECTion:EXTension:ENABle <ON | OFF>

Applicable Models: All

(Read-Write) Turns port extensions ON or OFF for all ports.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<ON | OFFl>

ON (or 1) - turns port extensions ON.

OFF (or 0) - turns port extensions OFF.

Examples

CALC:FSIM:DRAF:SECT:EXT:ENAB ON

calculate2:fsimulator:draft:section:extension:enable off

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:SECTion:EXTension:ENABle?

Return Type

Boolean (1 = ON, 0 = OFF)

Default

OFF


CALCulate<cnum>:FSIMulator:DRAFt:SECTion:ZCONversion:ENABle <ON | OFF>

Applicable Models: All

(Read-Write) Turns all ZConversions ON or OFF (both SE and BAL).    

Note:  This command affects ALL measurements on the specified channel.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<ON | OFFl>

ON (or 1) - turns all ZConversions ON.

OFF (or 0) - turns all ZConversions OFF.

Examples

CALC:FSIM:DRAF:SECT:ZCON:ENAB ON

calculate2:fsimulator:draft:section:zconversion:enable off

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:SECTion:ZCONversion:ENABle?

Return Type

Boolean (1 = ON, 0 = OFF)

Default

ON


CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:DIFFerential:STATe <bool>

Applicable Models: All

(Read-Write) Sets the differential port impedance conversion function ON/OFF. Must also set the fixture simulator function to ON using CALC:FSIM:STAT.

See Critical Note

Parameters

 

<cnum>

Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1.

<bool>

State of the differential port impedance conversion function. Choose from

OFF (or 0) Differential port impedance conversion OFF

ON (or 1) Differential port impedance conversion ON

Examples

CALC:FSIM:DRAF:ZCON:DIFF:STAT 1
calculate2:fsimulator:draft:zconversion:DIFFerential:state off

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:DIFFerential:STATe?

Return Type

Boolean

Default

OFF


CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:DIFFerential:BPORt<pnum>:COMPLex <real>,<img>

Applicable Models: All

(Read-Write) Sets the complex impedance value for the differential port impedance conversion function.

See Critical Note

Parameters

 

<cnum>

Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1.

<pnum>

Balanced port number. Choose from 1 to 999.

Note: See Balanced port versus Logical port.

<real>

Real part of the Impedance value in Units. Choose a number between 0 and 1E18

<img>

Imaginary part of the Impedance value in Units. Choose a number between 0 and 1E18.

Examples

CALC:FSIM:DRAF:ZCON:DIFF:BPOR2:COMPL 200,10
calculate2:fsimulator:draft:zconversion:differential:bport2:complex 20,3

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:DIFFerential:BPORt<pnum>:COMPlex?

Return Type

Comma-separated numeric

Default

0,0


CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:DIFFerential:BPORt<pnum>:SCALar <value>

Applicable Models: All

(Read-Write) Sets the real part of impedance value for the differential port impedance conversion function.

See Critical Note

Parameters

 

<cnum>

Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1.

<pnum>

Balanced port number. Choose from 1 to 999.

Note: See Balanced port versus Logical port.

<value>

Real part of the Impedance value in Units. Choose a number between 0 and 1E18

Examples

CALC:FSIM:DRAF:ZCON:DIFF:BPOR2:SCAL 200,10
calculate2:fsimulator:draft:zconversion:differential:bport2:scalar 20,3

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:DIFFerential:BPORt<pnum>:SCALer?

Return Type

Numeric

Default

1


CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:DIFFerential:LPORt<pnum>:COMPLex <real>,<img>

Applicable Models: All

(Read-Write) Sets the complex impedance value for the differential mode port impedance conversion function.

See Critical Note

Parameters

 

<cnum>

Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1.

<pnum>

Logical port number. Choose from 1 to 999.

Note: See Balanced port versus Logical port.

<real>

Real part of the Impedance value in Units. Choose a number between 0 and 1E18

<img>

Imaginary part of the Impedance value in Units. Choose a number between 0 and 1E18.

Examples

CALC:FSIM:DRAF:ZCON:DIFF:LPOR2:COMPL 200,10
calculate2:fsimulator:draft:zconversion:differential:lport2:complex 20,3

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:DIFFerential:LPORt<pnum>:COMPlex?

Return Type

Comma-separated numeric

Default

0,0


CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:DIFFerential::LPORt<pnum>:SCALar <value>

Applicable Models: All

(Read-Write) Sets the real part of impedance value for the differential:mode port impedance conversion function.

See Critical Note

Parameters

 

<cnum>

Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1.

<pnum>

logical port number. Choose from 1 to 999.

Note: See Balanced port versus Logical port.

<value>

Real part of the Impedance value in Units. Choose a number between 0 and 1E18

Examples

CALC:FSIM:DRAF:ZCON:COMM:LPOR2:DiFF 200,10
calculate2:fsimulator:draft:zconversion:differential:lport2:scalar 20,3

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:DIFFerential::LPORt<pnum>:SCALer?

Return Type

Numeric

Default

1


CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:COMMonmode:STATe <bool>

Applicable Models: All

(Read-Write) Sets the common mode port impedance conversion function ON/OFF. Must also set the fixture simulator function to ON using CALC:FSIM:STAT.

See Critical Note

Parameters

 

<cnum>

Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1.

<bool>

State of the differential port impedance conversion function. Choose from

OFF (or 0) Differential port impedance conversion OFF

ON (or 1) Differential port impedance conversion ON

Examples

CALC:FSIM:DRAF:ZCON:COMM:STAT 1
calculate2:fsimulator:draft:zconversion:commonmode:state off

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:COMMonmode:STATe?

Return Type

Boolean

Default

OFF


CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:COMMonmode:BPORt<pnum>:COMPLex <real>,<img>

Applicable Models: All

(Read-Write) Sets the complex impedance value for the common mode port impedance conversion function.

See Critical Note

Parameters

 

<cnum>

Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1.

<pnum>

Balanced port number. Choose from 1 to 999.

Note: See Balanced port versus Logical port.

<real>

Real part of the Impedance value in Units. Choose a number between 0 and 1E18

<img>

Imaginary part of the Impedance value in Units. Choose a number between 0 and 1E18.

Examples

CALC:FSIM:DRAF:ZCON:COMM:BPOR2:COMPL 200,10
calculate2:fsimulator:draft:zconversion:commonmode:bport2:complex 20,3

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:COMMonmode:BPORt<pnum>:COMPlex?

Return Type

Comma-separated numeric

Default

0,0


CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:COMMonmode:BPORt<pnum>:SCALar <value>

Applicable Models: All

(Read-Write) Sets the real part of impedance value for the common mode port impedance conversion function.

See Critical Note

Parameters

 

<cnum>

Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1.

<pnum>

Balanced port number. Choose from 1 to 999.

Note: See Balanced port versus Logical port.

<value>

Real part of the Impedance value in Units. Choose a number between 0 and 1E18

Examples

CALC:FSIM:DRAF:ZCON:COMM:BPOR2:SCAL 200
calculate2:fsimulator:draft:zconversion:commonmode:bport2:scalar 20

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:COMMonmode:BPORt<pnum>:SCALer?

Return Type

Numeric

Default

1


CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:COMMonmode:LPORt<pnum>:COMPLex <real>,<img>

Applicable Models: All

(Read-Write) Sets the complex impedance value for the common mode port impedance conversion function.

See Critical Note

Parameters

 

<cnum>

Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1.

<pnum>

Logical port number. Choose from 1 to 999.

Note: See Balanced port versus Logical port.

<real>

Real part of the Impedance value in Units. Choose a number between 0 and 1E18

<img>

Imaginary part of the Impedance value in Units. Choose a number between 0 and 1E18.

Examples

CALC:FSIM:DRAF:ZCON:COMM:LPOR2:COMPL 200,10
calculate2:fsimulator:draft:zconversion:commonmode:lport2:complex 20,3

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:COMMonmode:LPORt<pnum>:COMPlex?

Return Type

Comma-separated numeric

Default

0,0


CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:COMMonmode:LPORt<pnum>:SCALar <value>

Applicable Models: All

(Read-Write) Sets the real part of impedance value for the common mode port impedance conversion function.

See Critical Note

Parameters

 

<cnum>

Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1.

<pnum>

logical port number. Choose from 1 to 999.

Note: See Balanced port versus Logical port.

<value>

Real part of the Impedance value in Units. Choose a number between 0 and 1E18

Examples

CALC:FSIM:DRAF:ZCON:COMM:LPOR2:SCAL 200
calculate2:fsimulator:draft:zconversion:commonmode:lport2:scalar 20

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:COMMonmode:LPORt<pnum>:SCALer?

Return Type

Numeric

Default

1


CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:SENDed:PORT<pnum>:STATe <bool>

Applicable Models: All

(Read-Write) Sets the single-ended impedance conversion function ON/OFF. Must also set the fixture simulator function to ON using CALC:FSIM:STAT.

See Critical Note

Parameters

 

<cnum>

Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1.

<pnum>

Port number. Choose from 1 to 999.

<bool>

State of the single-ended port impedance conversion function. Choose from

OFF (or 0) single-ended  port impedance conversion OFF

ON (or 1) single-ended  port impedance conversion ON

Examples

CALC:FSIM:DRAF:ZCON:SEND:PORT3:STAT 1
calculate2:fsimulator:draft:zconversion:sended:port2:state off

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:SENDed:PORT:STATe?

Return Type

Boolean

Default

ON


CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:SENDed:PORTpnum>:COMPLex <real>,<img>

Applicable Models: All

(Read-Write) Sets the complex impedance value for the single-ended port impedance conversion function.

See Critical Note

Parameters

 

<cnum>

Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1.

<pnum>

Pport number. Choose from 1 to 999.

<real>

Real part of the Impedance value in Units. Choose a number between 0 and 1E18

<img>

Imaginary part of the Impedance value in Units. Choose a number between 0 and 1E18.

Examples

CALC:FSIM:DRAF:ZCON:SEND:POR2:COMPL 200,10
calculate2:fsimulator:draft:zconversion:sended:port2:complex 20,3

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:SENDed:PORT<pnum>:COMPlex?

Return Type

Comma-separated numeric

Default

0,0


CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:SENDed:PORT<pnum>:SCALer <val>

Applicable Models: All

(Read-Write) Sets the real part of impedance value for the single-ended port impedance conversion function.

See Critical Note

Parameters

 

<cnum>

Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1.

<pnum>

Pport number. Choose from 1 to 999.

<val>

Real part of the Impedance value in Units. Choose a number between 0 and 1E18

Examples

CALC:FSIM:DRAF:ZCON:SEND:PORT:SCAL 0
calculate2:fsimulator:draft:zconversion:sended:port2:scalar 20,3

Query Syntax

CALCulate<cnum>:FSIMulator:DRAFt:ZCONversion:SENDed:PORT<pnum>:SCALer?

Return Type

Numeric

Default

1