Applicable Models: N522xB, N523xB, N524xB, E5080A/B (Read-Write) Sets and returns the status of the LXI LAN status indicator on the LAN Status dialog. |
|
Parameters |
|
<bool> |
Choose from: OFF or 0 - Changes the LXI Status indicator to ‘NORMAL’ and closes the dialog if it was opened by this command. ON or 1 - Changes the LXI Status indicator to ‘IDENTIFY’ and opens the dialog if it was not already open. |
Examples |
LXI:IDEN
1 |
Query Syntax |
LXI:IDENtify[:STATe]? |
Return Type |
Boolean |
OFF |