When you use the PXI VNAs, you can control the M9379A amplifier through the VNA firmware. The following commands are available when the launcher includes the M9379A.
| SENSe:AMPLifier:M9379 | COUNt? | MODule | :CHASsis | :PATH | :SLOT 
 | 
Click on a keyword to view the command details.
| Applicable Models: PXI VNAs (Read-only) Returns the total number of M9379A amplifier modules that are connected to the VNA firmware. | |
| Parameters | 
 | 
| <cnum> | Any existing channel number; if unspecified, value is set to 1. This command is common for all channels and the setting is ignored. | 
| Examples | SENS:AMPL:M9379:COUN? | 
| Return Type | Numeric | 
| Default | Not applicable | 
| Applicable Models: PXI VNAs (Read-Write) Sets and reads the attenuation of the M9379A amplifier 1. | |
| Parameters | 
 | 
| <cnum> | Any existing channel number; if unspecified, value is set to 1. | 
| <mod> | Module number of M9379A. The number starts from 1 for the leftmost module of M9379A. | 
| <att> | Attenuation in dB from 0 to 28 with 2 step | 
| Examples | SENS:AMPL:M9379:MOD1:ATT 
		 10 | 
| Query Syntax | SENSe<cnum>:AMPLifier:M9379:MODule<mod>:ATTenuation? | 
| Return Type | Numeric | 
| 28 | |
| Applicable Models: PXI VNAs (Read Only) Returns the chassis number where the specified M9379A module is located. | |
| Parameters | 
 | 
| <cnum> | Any existing channel number; if unspecified, value is set to 1. This command is common for all channels and the setting is ignored. | 
| <mod> | Module number of M9379A. The number starts from 1 for the leftmost module of M9379A. | 
| Examples | SENS:AMPL:M9379:MOD1:CHAS? sense2:amplifier:m9379:module2:chassis? | 
| Return Type | Numeric | 
| Not applicable | |
| Applicable Models: PXI VNAs (Read-Write) Sets and reads the status of M9379A control. | |
| Parameters | 
 | 
| <cnum> | Any existing channel number; if unspecified, value is set to 1. | 
| <mod> | Module number of M9379A. The number starts from 1 for the leftmost module of M9379A. | 
| <bool> | Module control state. Choose from: O or OFF - Skips to control the M9379A at the specified channel. 1 or ON - Enables to control the M9379A at the specified channel. | 
| Examples | SENS:AMPL:M9379:MOD1:CONT ON sense2:amplifier:m9379:module2:control 0 | 
| Query Syntax | SENSe<cnum>:AMPLifier:M9379:MODule<mod>:CONTrol[:STATe]? | 
| Return Type | Boolean | 
| 1 or ON | |
| Applicable Models: PXI VNAs (Read-Write) Sets and reads the path for the M9379A amplifier 1. | |
| Parameters | 
 | 
| <cnum> | Any existing channel number; if unspecified, value is set to 1. | 
| <mod> | Module number of M9379A. The number starts from 1 for the leftmost module of M9379A. | 
| <char> | Path. Choose from: THRU - Through. AMPLifier - amplifier 1. NFReceiver - NF receiver switch (NF measurement only) | 
| Examples | SENS:AMPL:M9379:MOD1:PATH THRU sense2:amplifier:m9379:module2:path amplifier | 
| Query Syntax | SENSe<cnum>:AMPLifier:M9379:MODule<mod>:PATH? | 
| Return Type | Char | 
| THRU | |
| Applicable Models: PXI VNAs (Read-Write) Sets and reads the status of M9379A power. | |
| Parameters | 
 | 
| <cnum> | Any existing channel number; if unspecified, value is set to 1. This command is common for all channels and the setting is ignored. | 
| <mod> | Module number of M9379A. The number starts from 1 for the leftmost module of M9379A. | 
| <bool> | power control state. Choose from: 0 or OFF - Power off 1 or ON - Power on | 
| Examples | SENS:AMPL:M9379:MOD1:POW ON sense2:amplifier:m9379:module2:power 0 | 
| Query Syntax | SENSe<cnum>:AMPLifier:M9379:MODule<mod>:POWer[:STATe]? | 
| Return Type | Boolean | 
| 0 or OFF | |
| Applicable Models: PXI VNAs (Read Only) Reads the slot number where the M9379A is located. | |
| Parameters | 
 | 
| <cnum> | Any existing channel number; if unspecified, value is set to 1. This command is common for all channels and the setting is ignored. | 
| <mod> | Module number of M9379A. The number starts from 1 for the leftmost module of M9379A. | 
| Examples | SENS:AMPL:M9379:MOD1:SLOT? sense2:amplifier:m9379:module2:slot? | 
| Return Type | Numeric | 
| Not applicable | |
| Applicable Models: PXI VNAs (Read-Write) Sets and reads the path for the M9379A switch | |
| Parameters | 
 | 
| <cnum> | Any existing channel number; if unspecified, value is set to 1. | 
| <mod> | Module number of M9379A. The number starts from 1 for the leftmost module of M9379A. | 
| <char> | Path. Choose from: A - Path A B - Path B NFSource - NF source switch (NF measurement only) NFLO - NF LO switch (Option 720 only) NFReceiver - NF receiver switch (NF measurement only) | 
| Examples | SENS:AMPL:M9379:MOD1:SWIT:PATH A sense2:amplifier:m9379:module2:switch:path b | 
| Query Syntax | SENSe<cnum>:AMPLifier:M9379:MODule<mod>:SWITch:PATH? | 
| Return Type | <char> | 
| A | |