SENSe:BANDwidth | BWIDth Commands


SENSe:BANDwidth | BWIDth:

RESolution <num>

TRACk:FORCe

TRACk[:STATe] <bool>

See Also


SENSe<cnum>:BANDwidth | BWIDth[:RESolution] <num>

Applicable Models: All

(Read-Write) Sets the bandwidth of the digital IF filter to be used in the measurement. (Use either Sense:Bandwidth or Sense:Bwidth)

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<num>

IF Bandwidth in Hz. The list of valid IF Bandwidths is different depending on the VNA model. (Click to see the lists.) If an invalid number is specified, the analyzer will round up to the closest valid number.

This parameter supports MIN and MAX as arguments. Learn more.

Examples

SENS:BWID 1KHZ
sense2:bandwidth:resolution 1000

Query Syntax

SENSe<cnum>:BANDwidth | BWIDth[:RESolution]?

Return Type

Numeric

Default

Varies with VNA model.


SENSe<cnum>:BANDwidth | BWIDth:TRACk:FORCe <bool>

Applicable Models: N522xB, N5234B, N5235B, N524xB, E5080A/B

(Read-Write) Enables/disables the Reduce IF BW at Low Frequencies feature in segments with IFBW arbitrary.

(Use either Sense:Bandwidth:Track:Force or Sense:Bwidth:Track:Force).

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<bool>

Choose from:

ON or 1 -  Enable reduce IF BW at Low Frequencies in segments with IFBW arbitrary.

OFF or 0 - Disable reduce IF BW at Low Frequencies in segments with IFBW arbitrary.

Examples

SENS:BWID:TRAC:FORC OFF
sense2:bandwidth:track:force 1

Query Syntax

SENSe<cnum>:BANDwidth | BWIDth:TRACk:FORCe?

Return Type

Boolean

Default

OFF


SENSe<cnum>:BANDwidth | BWIDth:TRACk[:STATe] <bool>

Applicable Models: N522xB, N5234B, N5235B, N524xB, E5080A/B, M983xA

(Read-Write) Sets and returns the state of the Reduce IF BW at Low Frequencies feature.

(Use either Sense:Bandwidth:Track or Sense:Bwidth:Track).

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<bool>

Choose from:

ON or 1 -  Reduce IF BW at Low Frequencies is set ON

OFF or 0 - Reduce IF BW at Low Frequencies is set OFF

Examples

SENS:BWID:TRAC OFF
sense2:bandwidth:track 1

Query Syntax

SENSe<cnum>:BANDwidth | BWIDth:TRACk[:STATe]?

Return Type

Boolean

Default

OFF: E5080A

ON: other models