Vector Signal Analyzer Commands

Controls the connection between the VNA and the Vector Signal Analyzer (89600 VSA) Application.

SENSe:VSA

CONNect

     | [:STATe]

DATA

     | MOD

          | PIN1

               | [:STATe]

          | PINWav

              | [:STATE]

          | POU2

               | [:STATe]

     | STReam

          | [:STATe]

DTRigger

     | [:STATe]

FREQuency

     | CENTer

IF

     | OFFSet

LO

     | SIDE

SAVe

     | INCLude

          | [:STATe]

SHOW

SPECtrum

     | AUTOtune

STAtus

     | REPort?

 

Click on a red keyword to view the command details.

 

See Also


SENSe<ch>:VSA:CONNect[:STATe]

(Read-Write) Set and read the VNA to VSA connection state.

Parameters

 

<ch>

Any existing SA or MOD/MODX channel. If unspecified, value is set to 1.

<bool>

Choose from:

OFF (or 0)- Disconnect VNA from VSA 89600

ON (or 1)- Connect VNA to VSA 89600

Examples

SENS:VSA:CONN ON

Query Syntax

SENSe<ch>:VSA:CONNect[:STATe]?

Return Type

Boolean

Default

OFF


SENSe<ch>:VSA:DATA:MOD:PIN1[:STATe]

(Read-Write) Set to stream input power to a VSA measurement channel.

Parameters

 

<ch>

Any existing SA or MOD/MODX channel. If unspecified, value is set to 1.

<bool>

Choose from:

OFF (or 0) - Do not stream input power to VSA.

ON (or 1) - Stream input power to VSA.

Examples

SENS:VSA:DATA:MOD:PIN1 ON

Query Syntax

SENSe<ch>:VSA:DATA:MOD:PIN1[:STATe]?

Return Type

Boolean

Default

ON


SENSe<ch>:VSA:DATA:MOD:PINWav[:STATe]

(Read-Write) Set to stream ideal input power to VSA measurement channel.

Parameters

 

<ch>

Any existing SA or MOD/MODX channel. If unspecified, value is set to 1.

<bool>

Choose from:

OFF (or 0) - Do not stream ideal input power to VSA.

ON (or 1) - Stream ideal input power to VSA.

Examples

SENS:VSA:DATA:MOD:PINWav ON

Query Syntax

SENSe<ch>:VSA:DATA:MOD:PIN1[:STATe]?

Return Type

Boolean

Default

ON


SENSe<ch>:VSA:DATA:MOD:POU2[:STATe]

(Read-Write) Set to stream output power to a VSA measurement channel.

Parameters

 

<ch>

Any existing SA or MOD/MODX channel. If unspecified, value is set to 1.

<bool>

Choose from:

OFF (or 0) - Do not stream output power to VSA.

ON (or 1) - Stream output power to VSA.

Examples

SENS:VSA:DATA:MOD:POU2 ON

Query Syntax

SENSe<ch>:VSA:DATA:MOD:POU2[:STATe]?

Return Type

Boolean

Default

ON


SENSe<ch>:VSA:DATA:STReam[:STATe]

(Read-Write) Set and read the data stream state.

Parameters

 

<ch>

Any existing SA or MOD/MODX channel. If unspecified, value is set to 1.

<bool>

Choose from:

OFF (or 0) - Do not stream data from VNA to VSA.

ON (or 1) - Stream data from VNA to VSA.

Examples

SENS:VSA:DATA:STR ON

Query Syntax

SENSe<ch>:VSA:DATA:STReam[:STATe]?

Return Type

Boolean

Default

OFF


SENSe<ch>:VSA:DTRigger[:STATe]

(Read-Write) Set and read the state of the digital trigger. This command is used to make the time domain IQ exported data starting time identical sweep-to-sweep. Disabling this command makes the exported data less stable from sweep-to-sweep.

Parameters

 

<ch>

Any existing SA or MOD/MODX channel. If unspecified, value is set to 1.

<bool>

Choose from:

OFF (or 0)- Disable digital trigger.

ON (or 1)- Enable digital trigger.

Examples

SENS:VSA:DTR 1

Query Syntax

SENSe<ch>:VSA:DTRigger[:STATe]?

Return Type

Boolean

Default

ON


SENSe<ch>:VSA:FREQuency:CENTer

(Read-Write) Set and read the VSA center frequency which determines the LO frequency (LO Freq = VSA Center ± IF Offset) and the display center frequency of the VNA and VSA 89600.

Parameters

 

<ch>

Any existing SA or MOD/MODX channel. If unspecified, value is set to 1.

<num>

Center frequency. Choose any number between the minimum and maximum frequency limits of the analyzer. Units are Hz.

Examples

SENS:VSA:FREQ:CENT 6e9

Query Syntax

SENSe<ch>:VSA:FREQuency:CENTer?

Return Type

Numeric

Default

3.021e9


SENSe<ch>:VSA:IF:OFFSet

(Read-Write) Set and read the IF offset used for calculating the LO frequency.

Parameters

 

<ch>

Any existing SA or MOD/MODX channel. If unspecified, value is set to 1.

<num>

IF offset value in Hertz. The range is 0 to 21 MHz.

Examples

SENS:VSA:IF:OFFS 20e6

Query Syntax

SENSe<ch>:VSA:IF:OFFSet?

Return Type

Numeric

Default

21e6


SENSe<ch>:VSA:LO:SIDE

(Read-Write) Set and read the LO side.

Parameters

 

<ch>

Any existing SA or MOD/MODX channel. If unspecified, value is set to 1.

<enum>

Choose from:

LOW - LO Freq = VSA Center - IF Offset

HIGH - LO Freq = VSA Center + IF Offset

Examples

SENS:VSA:LO:SIDE LOW

Query Syntax

SENSe<ch>:VSA:LO:SIDE?

Return Type

Enumeration

Default

LOW


SENSe<ch>:VSA:SAVe:INCLude[:STATe]

(Read-Write) Sets to automatically save the VSA state file and embed it into the VNA state file (.csa file).

Parameters

 

<ch>

Any existing SA or MOD/MODX channel. If unspecified, value is set to 1.

<bool>

Choose from:

OFF (or 0)- Disable  the VSA state within VNA state file

ON (or 1)- Enable the VSA state within VNA state file

Examples

SENS:VSA:DTR 1

Query Syntax

SENSe<ch>:VSA:SAVe:INCLude[:STATe]?

Return Type

Boolean

Default

ON


SENSe<ch>:VSA:SHOW

(Write-only) Sets the VSA window in front of the VNA GUI when the VSA-to-VNA connection is running.

Parameters

 

<ch>

Any existing SA or MOD/MODX channel. If unspecified, value is set to 1.

Examples

SENS:VSA:SHOW

Default

Not Applicable


SENSe<ch>:VSA:SPECtrum:AUTOtune

(Write-only) Sets the VSA spectrum settings to match the current SA coherent repetition rate. In addition, it forces the VSA RBW to match the coherent tone spacing.

Parameters

 

<ch>

Any existing SA or MOD/MODX channel. If unspecified, value is set to 1.

Examples

SENS:VSA:SPEC:AUTO

Default

Not Applicable


SENSe<ch>:VSA:STAtus:REPort?

(Read-only) Reads the status of the VNA to VSA connection and configuration status. Learn more.

Parameters

 

<ch>

Any existing SA or MOD/MODX channel. If unspecified, value is set to 1.

Examples

SENS:VSA:STA:REP?

Return Type

Char