These commands control the compensation in the Impedance Measurement class.
SENSe:ZA CORRection:CSET:IMPort | FIXTure | SPARm FIXTURE | CKIT | OPEN | G | C | SHORt | R | L |
Click on a red keyword to view the command details.
See Also
Applicable Models: All with Impedance Measurement Options (S9x041B) (Read-Write) Sets and returns the ON |OFF state of Fixture Compensation .The Fixture Compensation data from the selected Cal Sets is enabled. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<bool> |
ON | OFF state. Choose from 0 - Fixture Compensation is disabled 1 - Fixture Compensation is enable |
Examples |
SENS:ZA:CORR:CSET:IMP:FIXT ON sense2:za:correction:cset:import:fixture 1 |
Query Syntax |
SENSe<cnum>:ZA:CORRection:CSET:IMPort:FIXTure? |
Return Type |
Boolean |
OFF |
Applicable Models: All with Impedance Measurement Options (S9x041B) (Read-Write) Sets and returns the ON |OFF state of S-Parameter calibration .The S-Parameter calibration data from the selected Cal Sets is enabled. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<bool> |
ON | OFF state. Choose from 0 - S-Parameter calibration is disabled 1 - S-Parameter calibration is enable |
Examples |
SENS:ZA:CORR:CSET:IMP:SPAR ON sense2:za:correction:cset:import:sparam 1 |
Query Syntax |
SENSe<cnum>:ZA:CORRection:CSET:IMPort:SPARm? |
Return Type |
Boolean |
OFF |
Applicable Models: All with Impedance Measurement Options (S9x041B) (Read-Write) This command selects the fixture (16198A-010) calibration data file (.dat) which is provided by Keysight. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
<FileName> |
calibration data file |
Examples |
SENS:ZA:FIXT:SEL
"C:\Fixture_Data_xxxxxxxxx.dat" |
Query Syntax |
SENSe<cnum>:ZA:FIXTure:SELect? |
Return Type |
String |
Default |
Null |
Applicable Models: All with Impedance Measurement Options (S9x041B) (Read-Write) This command sets/returns the G value of Open Standard for the fixture compensation. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
<value> |
G value of Open Standard |
Examples |
SENS:ZA:FIXT:CKIT:OPEN:G 1e-5 sense:za:fixture:ckit:open:g 1e-5 |
Query Syntax |
SENSe<cnum>:ZA:FIXTure:CKIT:OPEN:G? |
Return Type |
Numeric |
Default |
0 |
Applicable Models: All with Impedance Measurement Options (S9x041B) (Read-Write) This command sets/returns the capacitance value of Open Standard for the fixture compensation. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
<value> |
C value of Open Standard |
Examples |
SENS:ZA:FIXT:CKIT:OPEN:C 1e-5 sense:za:fixture:ckit:open:c 1e-5 |
Query Syntax |
SENSe<cnum>:ZA:FIXTure:CKIT:OPEN:C? |
Return Type |
Numeric |
Default |
0 |
Applicable Models: All with Impedance Measurement Options (S9x041B) (Read-Write) This command sets/returns the resistance value of Short Standard for the fixture compensation. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
<value> |
R value of Open Standard |
Examples |
SENS:ZA:FIXT:CKIT:SHOR:R 1e-5 sense:za:fixture:ckit:short:r 1e-5 |
Query Syntax |
SENSe<cnum>:ZA:FIXTure:CKIT:SHORt:R? |
Return Type |
Numeric |
Default |
0 |
Applicable Models: All with Impedance Measurement Options (S9x041B) (Read-Write) This command sets/returns the inductance value of Short Standard for the fixture compensation. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
<value> |
L value of Open Standard |
Examples |
SENS:ZA:FIXT:CKIT:SHOR:L 1e-5 sense:za:fixture:ckit:short:l 1e-5 |
Query Syntax |
SENSe<cnum>:ZA:FIXTure:CKIT:SHORt:L? |
Return Type |
Numeric |
Default |
0 |
Applicable Models: All with Impedance Measurement Options (S9x041B) (Read-Write) This command sets/returns the port for the impedance |
|
Parameters |
|
<cnum> |
Channel number of the measurement. If unspecified, <cnum> is set to 1. |
<string> |
Port number |
Examples |
SENS:ZA:PORT "1" sense:za:port "2" |
Query Syntax |
SENSe<cnum>:ZA:PORT? |
Return Type |
Numeric |
Default |
"1" |