Controls and queries settings that affect Millimeter Wave measurements.
See Also
Applicable Models: N5261A, N5262A, N5252A, N5292A (Read-Write) Set and return the active configuration. Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONF:ACTive command is executed. |
|
Parameters |
|
<string> |
The name of the mmWave configuration to activate. |
Examples |
SYST:CONF:MWAV:CONF:ACT "N5291A Broadband" 'Set to broadband configuration SYST:CONF:MWAV:CONF:ACT "WR10" 'Set to banded configuration system:configure:mwave:conf:active "Standard PNA" 'Set to standard PNA configuration |
Query Syntax |
SYSTem:CONFigure:MWAVe:CONF:ACTive? |
Return Type |
String |
Default |
Not applicable |
Applicable Models: N5293A, N5295A (Read-only) Return the calibration date of the active configuration's test set. Three integers are returned (year,month,day). All three integers will be 0 if there is no calibration data for the active test set. |
|
Parameters |
None |
Examples |
SYST:CONF:MWAV:CONF:ACT:CAL:DATE? system:configure:mwave:conf:active:calibration:date? |
Return Type |
Integer |
Default |
Not applicable |
Applicable Models: N5293A, N5295A (Read-only) Return the calibration time of the active configuration's test set. Three integers are returned (hour,minute,second). All three integers will be 0 if there is no calibration data for the active test set. |
|
Parameters |
None |
Examples |
SYST:CONF:MWAV:CONF:ACT:CAL:TIME? system:configure:mwave:conf:active:calibration:time? |
Return Type |
Integer |
Default |
Not applicable |
Applicable Models: N5293A, N5295A (Read-only) Return the model number of the active test set. |
|
Parameters |
None |
Examples |
SYST:CONF:MWAV:CONF:ACT:MOD? system:configure:mwave:conf:active:model? |
Return Type |
String |
Default |
Not applicable |
Applicable Models: N5293A, N5295A (Read-only) Return the option number of the active test set. |
|
Parameters |
None |
Examples |
SYST:CONF:MWAV:CONF:ACT:OPT? system:configure:mwave:conf:active:option? |
Return Type |
String |
Default |
Not applicable |
Applicable Models: N5293A, N5295A (Read-only) Return the calibration date of the active configuration's port. Three integers are returned (year,month,day). All three integers will be 0 if there is no calibration data for the active port. |
|
Parameters |
None |
Examples |
SYST:CONF:MWAV:CONF:ACT:PORT1:CAL:DATE? system:configure:mwave:conf:active:port1:calibration:date? |
Return Type |
Integer |
Default |
Not applicable |
Applicable Models: N5293A, N5295A (Read-only) Return the calibration time of the active configuration's port. Three integers are returned (hour,minute,second). All three integers will be 0 if there is no calibration data for the active port. |
|
Parameters |
None |
Examples |
SYST:CONF:MWAV:CONF:ACT:PORT1:CAL:TIME? system:configure:mwave:conf:active:port1:calibration:time? |
Return Type |
Integer |
Default |
Not applicable |
Applicable Models: N5293A, N5295A (Read-only) Return the model number of the frequency extender module connected to the specified port number. |
|
Parameters |
None |
Examples |
SYST:CONF:MWAV:CONF:ACT:PORT1:MOD? system:configure:mwave:conf:active:port1:model? |
Return Type |
String |
Default |
Not applicable |
Applicable Models: N5293A, N5295A (Read-only) Return the option number of the frequency extender module connected to the specified port number. |
|
Parameters |
None |
Examples |
SYST:CONF:MWAV:CONF:ACT:PORT1:OPT? system:configure:mwave:conf:active:port1:option? |
Return Type |
String |
Default |
Not applicable |
Applicable Models: N5293A, N5295A (Read-only) Return the serial number of the frequency extender module connected to the specified port number. |
|
Parameters |
None |
Examples |
SYST:CONF:MWAV:CONF:ACT:PORT1:SER? system:configure:mwave:conf:active:port1:serial? |
Return Type |
String |
Default |
Not applicable |
Applicable Models: N5292A (Read-only) Return the serial number of the test set. |
|
Parameters |
None |
Examples |
SYST:CONF:MWAV:CONF:ACT:SER? system:configure:mwave:conf:active:serial? |
Return Type |
String |
Default |
Not applicable |
Applicable Models: N5261A, N5262A, N5252A, N5292A (Read-Write) Add a banded mmWave configuration. |
|
Parameters |
|
<string> |
The name of the mmWave configuration to add. |
Examples |
SYST:CONF:MWAV:CONF:ADD "WR10" system:configure:mwave:conf:add "wr10" |
Query Syntax |
SYSTem:CONFigure:MWAVe:CONF:ADD? |
Return Type |
String |
Default |
Not applicable |
Applicable Models: N5261A, N5262A, N5252A, N5292A (Read-only) Returns the list of mmWave configurations. |
|
Parameters |
|
Examples |
SYST:CONF:MWAV:CONF:CAT? system:configure:mwave:conf:catalog? |
Return Type |
Comma-delimited string. |
Default |
Not applicable |
Applicable Models: N5261A, N5262A, N5252A, N5292A (Write-only) Remove a mmWave configuration. |
|
Parameters |
|
<string> |
The name of the mmWave configuration to remove. |
Examples |
SYST:CONF:MWAV:CONF:REM "WR10" system:configure:mwave:conf:remove "wr10" |
Return Type |
Not applicable |
Default |
Not applicable |
Applicable Models: N5261A, N5262A, N5252A, N5292A (Read-Write) Set and read the LO multiplier value for the specified configuration. The LO Frequency Range multiplied by this value equals the test port frequency. Learn more about frequency settings. Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONF:ACTive command is executed. |
|
Parameters |
|
<string> |
The name of the mmWave configuration. |
<value> |
Choose a value within the range of the analyzer. |
Examples |
SYST:CONF:MWAV:FREQ:LO:MULT "WR10",8 system:configure:mwave:frequency:lo:multiplier "WR10",8 |
Query Syntax |
SYSTem:CONFigure:MWAVe:FREQuency:LO:MULTiplier? "WR10" |
Return Type |
Integer |
Default |
1 |
Applicable Models: N5261A, N5262A, N5292A (Read-Write) Set and read the LO source for the specified configuration. Learn more. Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONF:ACTive command is executed. |
|
Parameters |
|
<string> |
The name of the mmWave configuration. |
<source> |
The name of the LO source. |
Examples |
SYST:CONF:MWAV:FREQ:LO:SOUR "WR10","LO_Source" system:configure:mwave:frequency:lo:source "WR10","LO_Source" |
Query Syntax |
SYSTem:CONFigure:MWAVe:FREQuency:LO:SOURce? "WR10" |
Return Type |
String |
Default |
Internal LO source |
Applicable Models: N5261A, N5262A, N5252A, N5292A (Read-only) Return the calculated LO start frequency using the LO multiplier for the specified configuration. Learn more about frequency settings. |
|
Parameters |
|
<string> |
The name of the mmWave configuration. |
Examples |
SYST:CONF:MWAV:FREQ:LO:STAR? "WR10" system:configure:mwave:frequency:lo:start? "WR10" |
Return Type |
Double |
Default |
Dependent on the range of the analyzer |
Applicable Models: N5261A, N5262A, N5252A, N5292A (Read-only) Return the calculated LO stop frequency using the LO multiplier for the specified configuration. Learn more about frequency settings. |
|
Parameters |
|
<string> |
The name of the mmWave configuration. |
Examples |
SYST:CONF:MWAV:FREQ:LO:STOP? "WR10" system:configure:mwave:frequency:lo:stop? "WR10" |
Return Type |
Double |
Default |
Dependent on the range of the analyzer |
Applicable Models: N5261A, N5262A, N5252A, N5292A (Read-Write) Set and read the RF multiplier value for the specified configuration. The RF Frequency Range multiplied by this value equals the test port frequency range. Learn more about frequency settings. Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONF:ACTive command is executed. |
|
Parameters |
|
<string> |
The name of the mmWave configuration. |
<value> |
Choose a value within the range of the analyzer. |
Examples |
SYST:CONF:MWAV:FREQ:RF:MULT "WR10",6 system:configure:mwave:frequency:rf:multiplier "WR10",6 |
Query Syntax |
SYSTem:CONFigure:MWAVe:FREQuency:RF:MULTiplier? "WR10" |
Return Type |
Integer |
Default |
1 |
Applicable Models: N5261A, N5262A, N5292A (Read-Write) Set and read the RF source for the specified configuration. Learn more. Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONF:ACTive command is executed. |
|
Parameters |
|
<string> |
The name of the mmWave configuration. |
<source> |
The name of the RF source. |
Examples |
SYST:CONF:MWAV:FREQ:RF:SOUR "WR10","RF_Source" system:configure:mwave:frequency:rf:source "WR10","RF_Source" |
Query Syntax |
SYSTem:CONFigure:MWAVe:FREQuency:RF:SOURce? "WR10" |
Return Type |
String |
Default |
Internal RF source |
Applicable Models: N5261A, N5262A, N5252A, N5292A (Read-only) Return the calculated RF start frequency using the RF multiplier for the specified configuration. Learn more about frequency settings. |
|
Parameters |
|
<string> |
The name of the mmWave configuration. |
Examples |
SYST:CONF:MWAV:FREQ:RF:STAR? "WR10" system:configure:mwave:frequency:rf:start? "WR10" |
Return Type |
Double |
Default |
Dependent on the range of the analyzer |
Applicable Models: N5261A, N5262A, N5252A, N5292A (Read-only) Return the calculated RF stop frequency using the RF multiplier for the specified configuration. Learn more about frequency settings. |
|
Parameters |
|
<string> |
The name of the mmWave configuration. |
Examples |
SYST:CONF:MWAV:FREQ:RF:STOP? "WR10" system:configure:mwave:frequency:rf:stop? "WR10" |
Return Type |
Double |
Default |
Dependent on the range of the analyzer |
Applicable Models: N5261A, N5262A, N5252A, N5292A (Read-Write) Set and read the start frequency for the specified configuration. Learn more about frequency settings. Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONF:ACTive command is executed. |
|
Parameters |
|
<string> |
The name of the mmWave configuration. |
<value> |
The start frequency. |
Examples |
SYST:CONF:MWAV:FREQ:STAR "WR10",75e9 system:configure:mwave:frequency:start "WR10",75e9 |
Query Syntax |
SYSTem:CONFigure:MWAVe:FREQuency:STAR? "WR10" |
Return Type |
Double |
Default |
Dependent on the range of the analyzer |
Applicable Models: N5261A, N5262A, N5252A, N5292A (Read-Write) Set and read the stop frequency for the specified configuration. Learn more about frequency settings. Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONF:ACTive command is executed. |
|
Parameters |
|
<string> |
The name of the mmWave configuration. |
<value> |
The stop frequency. |
Examples |
SYST:CONF:MWAV:FREQ:STOP "WR10",110e9 system:configure:mwave:frequency:stop "WR10",110e9 |
Query Syntax |
SYSTem:CONFigure:MWAVe:FREQuency:STOP? "WR10" |
Return Type |
Double |
Default |
Dependent on the range of the analyzer |
Applicable Models: N5290A, N5291A (Read-only) Return the serial number of the mmWave system. |
|
Parameters |
None |
Examples |
SYST:CONF:MWAV:SER? system:configure:mwave:serial? "M42147691962" |
Return Type |
String |
Default |
Not applicable |
Applicable Models: N5261A, N5262A (Read-Write) Enable or disable automatic power leveling for the specified configuration. Learn more about test set properties. Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONF:ACTive command is executed. |
|
Parameters |
|
<string> |
The name of the mmWave configuration. |
<bool> |
Choose from: 0 - OFF - Disable automatic power leveling control. 1 - ON - Enable automatic power leveling control. |
Examples |
SYST:CONF:MWAV:TSET:ALC "WR10",1 system:configure:mwave:tset:alc "WR10",1 |
Query Syntax |
SYSTem:CONFigure:MWAVe:TSET:ALC? "WR10" |
Return Type |
Boolean |
Default |
1 |
Applicable Models: N5261A, N5262A, N5292A (Read-only) Returns the list of available test set names. |
|
Parameters |
|
Examples |
SYST:CONF:MWAV:TSET:CAT? system:configure:mwave:tset:catalog? |
Return Type |
Comma-delimited string. |
Default |
Not applicable |
Applicable Models: N5261A, N5262A, N5292A (Read-Write) Enable or disable mmWave mixer mode to allow mixer testing using the specified configuration. Learn more about test set properties. Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONF:ACTive command is executed. |
|
Parameters |
|
<string> |
The name of the mmWave configuration. |
<bool> |
Choose from: 0 - OFF - Disable mmWave mixer mode. 1 - ON - Enable mmWave mixer mode. |
Examples |
SYST:CONF:MWAV:TSET:MIXer "WR10",0 system:configure:mwave:tset:mixer "WR10",0 |
Query Syntax |
SYSTem:CONFigure:MWAVe:TSET:MIXer? "WR10" |
Return Type |
Boolean |
Default |
0 |
Applicable Models: N5261A, N5262A, N5292A (Read-Write) Set and read the test set name for the specified configuration. Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONF:ACTive command is executed. Setting the test set name may reset the test set properties to default values, which includes the following:
|
|
Parameters |
|
<string> |
The name of the mmWave configuration. |
<name> |
The name of the test set. |
Examples |
SYST:CONF:MWAV:TSET:NAME "WR10","N5262A" system:configure:mwave:tset:name "WR10","N5262A" |
Query Syntax |
SYSTem:CONFigure:MWAVe:TSET:NAME? "WR10" |
Return Type |
String |
Default |
Not applicable |
Applicable Models: N5261A, N5262A, N5292A (Read-Write) This command enables or disables modules for individual ports on a particular configuration. If an N5292A test set is attached it will detect if a module is physically present and only allow this command on those ports. Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONF:ACTive command is executed. |
|
Parameters |
|
<port> |
Test set port number. |
<configuration> |
The name of the mmWave configuration. Use SYSTem:CONFigure:MWAVe:CONF:CATalog? for a list of configuration names. |
<val> |
Enable/disable test set port. Choose from: 0 - OFF - Disable test set port. 1 - ON - Enable test set port. |
Examples |
SYST:CONF:MWAV:TSET:PORT1 "WR10",1 system:configure:mwave:tset:port1 "WR10",1 |
Query Syntax |
SYSTem:CONFigure:MWAVe:TSET:PORT1? "N5291A Broadband" |
Return Type |
Boolean |
Default |
0 |
Applicable Models: N5261A, N5262A, N5292A (Read-only) Return the number of ports on a test set. Only the test set ports having frequency extenders attached are detected. |
|
Parameters |
|
<string> |
The name of the mmWave configuration. |
Examples |
SYST:CONF:MWAV:TSET:PORT:COUNt? "N5291A Broadband" system:configure:mwave:tset:port:count? "N5291A Broadband" |
Return Type |
Integer |
Default |
Not applicable |
Applicable Models: N5261A, N5262A, N5252A, N5292A (Read-Write) Set and read the test set power limit for the specified configuration. Learn more about test set properties. Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONF:ACTive command is executed. |
|
Parameters |
|
<string> |
The name of the mmWave configuration. |
<value> |
The power limit. Choose a value between -90 and +13 dBm. |
Examples |
SYST:CONF:MWAV:TSET:POW:LIM "WR10",11 system:configure:mwave:tset:power:limit "WR10",11 |
Query Syntax |
SYSTem:CONFigure:MWAVe:TSET:POWer:LIMit? "WR10" |
Return Type |
Double |
Default |
11 dBm |
Applicable Models: N5261A, N5262A, N5252A, N5292A (Read-Write) Set and read the test set power offset for the specified configuration. Learn more about test set properties. Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONF:ACTive command is executed. |
|
Parameters |
|
<string> |
The name of the mmWave configuration. |
<value> |
The power offset. Choose a value between -30 and +30 dB. |
Examples |
SYST:CONF:MWAV:TSET:POW:OFFS "WR10",0 system:configure:mwave:tset:power:offset "WR10",0 |
Query Syntax |
SYSTem:CONFigure:MWAVe:TSET:POWer:OFFSet? "WR10" |
Return Type |
Double |
Default |
0 dB |
Applicable Models: N5261A, N5262A, N5252A, N5292A (Read-Write) Set and read the test set power slope for the specified configuration. Learn more about test set properties. Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONF:ACTive command is executed. |
|
Parameters |
|
<string> |
The name of the mmWave configuration. |
<value> |
The power slope. Choose a value between -2 dB/GHz and +2 dB/GHz. |
Examples |
SYST:CONF:MWAV:TSET:POW:SLOP "WR10",.113 system:configure:mwave:tset:power:slope "WR10",.113 |
Query Syntax |
SYSTem:CONFigure:MWAVe:TSET:POWer:SLOpe? "WR10" |
Return Type |
Double |
Default |
0.113 dB/GHz |
Applicable Models: N5261A, N5262A (Read-Write) Set and read the status of the RF power routing to the rear panel "SW SRC OUT" connector for the specified configuration. Note: Any changes to configuration settings are not active until the SYSTem:CONFigure:MWAVe:CONF:ACTive command is executed. |
|
Parameters |
|
<string> |
The name of the mmWave configuration. |
<bool> |
Choose from: 0 - OFF - Disable RF power routing to rear panel. 1 - ON - Enable RF power routing to rear panel "SW SRC OUT" connector. |
Examples |
SYST:CONF:MWAV:TSET:RPAN "WR10",1 system:configure:mwave:tset:rpanel "WR10",1 |
Query Syntax |
SYSTem:CONFigure:MWAVe:TSET:RPANel? "WR10" |
Return Type |
Boolean |
Default |
1 |