This VB Script program configures an External Source.
Learn more about External Source Configuration
These programs can be run as a macro in the VNA. To do this, copy the code into a text editor file such as Notepad and save on the VNA hard drive as ExtSource.vbs. Learn how to setup and run the macro.
External Device Configuration Commands
| ' Get the VNA application, and ' start the scpi parser, and preset the VNA dim app Set app = CreateObject("AgilentPNA835x.Application") set scpi = app.ScpiStringParser scpi.parse "*rst" ‘Configure the external source scpi.parse "Syst:conf:edev:add 'newSource'" scpi.parse "Syst:conf:edev:dtype 'newSource', 'Source'" scpi.parse "Syst:conf:edev:driver 'newSource', 'AGMXG'" scpi.parse "Syst:conf:edev:ioconfig 'newSource', 'gpib0::16::instr'" 'Activate and enable the external source scpi.parse "Syst:conf:edev:ioen 'newSource', 1" 'State activates and talks to the device if "Syst:conf:edev:ioen" is enabled scpi.parse "Syst:conf:edev:stat 'newSource', 1" |