SYSTem:CONFigure:EDEVice Commands


Configures and makes settings for an external device.

SYSTem:CONFigure:EDEVice:

| ADD

| CAT?

| CHANnel

     | BASE?

     | COUNt?

     | NAME?

     | NUMBer?

     | STATe

     | SYNC

| DRIVer

| DTYPe

| EXISts?

| IOConfig

| IOENable

| LOAD

| RCLock

    | VNA

        | STATe

| REMove

| SAVE

| SMU

     | CHANnel

          | STATe

| STATe

| TOUT

 

| DC  More commands

| PMAR  More commands

| PULSe  More commands

 

| SOURce:

     | DPPoint

     | HYBRid

          | INPut

               | FREQuency:CARRier

               | FREQency:MULTiplier

               | NAME

               | POWer:LIMit

               | PULSe:ENABle

          | LO

               | FREQuency:MULTiplier

               | NAME

               | POWer

               | PULSe:ENABle

          | LOCK:STATe

          | OUTPut

               | FREQuency:MAX

               | FREQuency:MIN

               | GAIN

               | MIXer:SIDeband

          | TYPE

     | MODulation

          | CONTrol

               | :STATe

     | TMODe

     | TPORt

 

Click on a red keyword to view the command details.

See Also


SYSTem:CONFigure:EDEVice:ADD <name>

Applicable Models: All

(Write-only) Adds an external device to the list of configured devices.  This is the same as pressing New on the Select an external device dialog.

Upon creation, all settings on the new device are set to the defaults. The device is not active until set using SYST:CONF:EDEV:STAT

Parameters

 

<name>

String - Model and type of the external device.

To see a list of configured external devices, use SYST:CONF:EDEV:CAT?

Examples

SYST:CONF:EDEV:ADD "myDevice"

system:configure:edevice:add "myDevice"

Query Syntax

Not Applicable

Default

Not Applicable


SYSTem:CONFigure:EDEVice:CAT?

Applicable Models: All

(Read-only) Returns a list of names of all configured devices. These are devices that appear in the external devices dialog.

Use SENS:FOM:CAT? to report all active devices.

Use Source:CAT? to report all active sources.

Parameters

None

Example

SYST:CONF:EDEV:CAT?

system:configure:edevice:cat

Return Type

String of comma-separated devices. "Device0:Driver0, Device1:Driver1"

Default

Not applicable


SYSTem:CONFigure:EDEVice:CHANnel<cnum>:BASE? <decoratedName>

Applicable Models: All

(Read-only) Returns the base name from the decorated name. For example, "N5186A Ch 3" returns N5186A.

See also, the Enable Output feature of the External Source Device dialog.

Parameters

 

<cnum>

Channel number of the external device. Ignored for this query.

<decoratedName>

String

Example

SYST:CONF:EDEV:CHAN:BASE? "myDevice"

Return Type

String

Default

Not applicable


SYSTem:CONFigure:EDEVice:CHANnel<cnum>:COUNt? <deviceName>

Applicable Models: All

(Read-only) This returns the total number of channels possible. Currently, this is always 4.

See also, the Enable Output feature of the External Source Device dialog.

Parameters

 

<cnum>

Channel number of the external device. Ignored for this query.

<deviceName>

String

Example

SYST:CONF:EDEV:CHAN:COUNt? "myDevice"

Return Type

Numeric

Default

Not applicable


SYSTem:CONFigure:EDEVice:CHANnel<cnum>:NAME? <deviceName>

Applicable Models: All

(Read-only) Returns the decorated name of the device for a particular channel. For example, SYST:CONF:EDEV:CHAN3:NAME? "N5186A" returns N5186A Ch 3.

See also, the Enable Output feature of the External Source Device dialog.

Parameters

 

<cnum>

Channel number of the external device.

<deviceName>

String

Example

SYST:CONF:EDEV:CHAN:NAME? "myDevice"

Return Type

String

Default

Not applicable


SYSTem:CONFigure:EDEVice:CHANnel<cnum>:NUMBer? <decoratedName>

Applicable Models: All

(Read-only) Returns the channel number from the decorated name. For example: "N5186A Ch 3" returns 3.

See also, the Enable Output feature of the External Source Device dialog.

Parameters

 

<cnum>

Channel number of the external device. Ignored for this query.

<decoratedName>

String

Example

SYST:CONF:EDEV:CHAN:NUMBer? "myDevice"

Return Type

String

Default

Numeric


SYSTem:CONFigure:EDEVice:CHANnel<cnum>[:STATe] <deviceName>,<value>

Applicable Models: All

(Read-only) Turns on or off channels on a particular external source.

See also, the Enable Output feature of the External Source Device dialog.

Parameters

 

<cnum>

Channel number of the external device.

<deviceName>

String

<value>

Boolean - Choose from:

OFF or 0 - Device communication disabled

ON or 1 - Device communication enabled

Example

SYST:CONF:EDEV:CHAN3 "myDevice",1

Query Syntax

SYSTem:CONFigure:EDEVice:CHANnel:STATe? <myDevice>

Return Type

Boolean

Default

Not applicable


SYSTem:CONFigure:EDEVice:CHANnel:SYNC <deviceName>,<value>

Applicable Models: All

(Read-only) Turns on or off channel phase synchronization on an external source supporting this feature.

See also, the Enable Output feature of the External Source Device dialog.

Parameters

 

<deviceName>

String

<value>

Boolean - Choose from:

OFF or 0 - Channel synchronization disabled

ON or 1 - Channel synchronization enabled

Example

SYST:CONF:EDEV:CHAN:SYNC "myDevice",1

Query Syntax

SYSTem:CONFigure:EDEVice:CHANnel:SYNC? <myDevice>

Return Type

Boolean

Default

OFF


SYSTem:CONFigure:EDEVice:DRIVer <name>,<value>

Applicable Models: All

(Read-Write) Sets and returns the external device driver (model).

Parameters

 

<name>

String - Name of the device.

<value>

String - External device driver (model). Choose from the following:

"AGPM" for all power meters.

"AGPULSEGEN" for supported pulse generators.

"DCSource" for all supported DC Sources

"DCMeter" for all supported DC Meters

See a list of supported external source drivers.

Examples

SYST:CONF:EDEV:DRIV "myDevice","AGPM"

system:configure:edevice:driver "myDevice","AGESG"

Query Syntax

SYSTem:CONFigure:EDEVice:DRIVer? <name>

Return Type

String

Default

"AGGeneric"


SYSTem:CONFigure:EDEVice:DTYPe <name>,<type>

Applicable Models: All

(Read-Write) Sets and returns the Device Type for the external device.

Parameters

 

<name>

String - Name of the device to modify.

<type>

String - Device type - not case sensitive. Choose from:

"None"

"Source" - external source

"Power Meter" - power meter

"DC Meter" - DC voltmeter

"DC Source" - DC power supply

"Pulse Generator" - external pulse generator

"SMU" - Source Measure Unit

Examples

SYST:CONF:EDEV:DTYP "myDevice","Power Meter"

system:configure:edevice:dtype "myDevice","Source"

Query Syntax

SYSTem:CONFigure:EDEVice:DTYPe? <name>

Return Type

String

Default

Source


SYSTem:CONFigure:EDEVice:EXISts? <string>

Applicable Models: All

(Read-only) Returns whether the named device is present on the bus for which it is configured.

Parameters

 

<string>

Name of the external device.

Example

SYST:CONF:EDEV:EXIS? "MyPowerMeter"

Return Type

Boolean

  • 0 - The device is not in the collection or the device fails to respond and times out when communication is attempted.

  • 1 - The device responds when communication is attempted.

Default

Not applicable


SYSTem:CONFigure:EDEVice:IOConfig <name>,<value>

Applicable Models: All

(Read-Write) Sets and return the configuration path for the specified external device.

Parameters

 

<name>

String - Name of the device.

<value>

String - Configuration path. Any valid VISA resource shown in the IO Configuration field of the external devices dialog, enclosed in quotes.

Use the SYST:COMM:VISA:RDEV:FIND? command to return IO devices that the visa subsystem can identify. This command will return addresses for devices found on GPIB, USB, or LAN.

Examples

SYST:CONF:EDEV:IOC "myDevice","GPIB0::13::INSTR"

SYST:CONF:EDEV:IOC "myDevice","TCPIP0::141.121.148.119::inst0::INSTR"

system:configure:edevice:ioconfig "myDevice","USB0::10893::19457::MZ00703073::0::INSTR"

Query Syntax

SYSTem:CONFigure:EDEVice:IOConfig? <name>

Return Type

String

Default

"" Empty String


SYSTem:CONFigure:EDEVice:IOENable <name>,<value>

Applicable Models: All

(Read-Write)  Enable or disable communication with an external device.

When disabled (OFF), the VNA will NOT attempt to connect to the external device regardless of the instrument state command (SYST:CONF:EDEV:STATe).  Therefore, no errors will be produced if the device is not connected.

This command is useful for debugging and testing states when the external device is not connected. This command is unnecessary in ordinary operation (when the device is connected).

Parameters

 

<name>

String - Name of the device.

<value>

Boolean - Choose from:

OFF or 0 - Device communication disabled

ON or 1 - Device communication enabled

Examples

SYST:CONF:EDEV:IOEN "myDevice", ON

system:configure:edevice:ioenable "myDevice", 0

Query Syntax

SYSTem:CONFigure:EDEVice:IOENable? <name>

Return Type

Boolean

Default

ON


SYSTem:CONFigure:EDEVice:LOAD <file>,<name>

Applicable Models: All

(Write-only) Recalls an external device configuration file from the VNA hard drive.

Currently, only DC Supply and DC Meter configuration files are supported. See more DC Device commands.

Use SYST:CONF:EDEV:SAVE to save a configuration file.

Parameters

 

<file>

String - Filename of the external device configuration file.

  1. If <file> is not a full path, it is assumed to be a relative path based at "D:\Drivers".

  2. The file specified using <file> cannot be the same file as "D:\Drivers\<name>.xml".

<name>

String - Name of the external device. Currently, only DC Supply and DC Meter configuration files are supported.

Examples

SYST:CONF:EDEV:LOAD "D:\Drivers\MyConfigFile.xml","MyDevice"

Query Syntax

Not Applicable

Default

Not Applicable


SYSTem:CONFigure:EDEVice:RCLock:VNA:STATe <name>,<state>

Applicable Models: All

(Read-Write) Set and return if VNA is Reference Clock Provider for the specified external device. 

Parameters

 

<name>

String - Name of the device. 

<state>  

Boolean - Choose from:

OFF or 0 - VNA is NOT Reference Clock Provider

ON or 1 - VNA is Reference Clock Provider

Examples

SYST:CONF:EDEV:RCL:VNA:STAT "myDevice",1

system:configure:edevice:rclock:vna:state "myDevice",0

Query Syntax

SYSTem:CONFigure:EDEVice:RCLock:VNA:STATe? <name>

Retrun Type 

Boolean

Default

0


SYSTem:CONFigure:EDEVice:REMove <name>

Applicable Models: All

(Write-only) Removes the specified device from the list of configured devices.  If the device is a Source and both Active and I/O Enabled is checked (ON), then the RF power state is set to OFF. Learn more.

Parameters

 

<name>

String - Name of the device. Not case sensitive. Use SYST:CONF:EDEV:CAT? to return a list of configured devices.

Examples

SYST:CONF:EDEV:REM "myDevice"

system:configure:edevice:remove "myDevice"

Query Syntax

Not Applicable

Default

Not Applicable


SYSTem:CONFigure:EDEVice:SAVE <file>,<name>

Applicable Models: All

(Write-only) Saves an external device configuration file to the VNA hard drive.

Currently, only DC Supply and DC Meter configuration files are supported. See more DC Device commands.

Use SYST:CONF:EDEV:LOAD to recall a configuration file.

Parameters

 

<file>

String - Filename of the external device configuration file.

<name>

String - Name of the external device.  Currently, only DC Supply and DC Meter configuration files are supported.

Examples

SYST:CONF:EDEV:SAVE "myDevice.xml","MyDCSupply"

Query Syntax

Not Applicable

Default

Not Applicable


SYSTem:CONFigure:EDEVice:SMU:CHANnel[1-4]:STATe <name>,<state>

Applicable Models: All

(Read-Write)  Set and return the state of activation of the SMU device channel. Learn more about configuring an external SMU.

When SYST:CONF:EDEV:IOEN = ON, and this command is set to ON, the VNA will attempt communication with the external device.

Send this command AFTER sending other external device settings (especially SYST:CONF:EDEV:DTYP) to avoid communicating with the device before it has been fully configured.

See Also: SYST:PREF:ITEM:EDEV:DPOL - Determines whether external devices remain activated or are de-activated when the VNA is Preset or when a Instrument State is recalled.

Parameters

 

<name>

String - Name of the SMU device.

<state>

Boolean - Choose from:

OFF or 0 - SMU Device channel  is NOT activated

ON or 1 - SMU Device channel is activated.

Examples

SYST:CONF:EDEV:SMU:CHAN2:STAT "myDevice", ON

system:configure:edevice:smu:channel2:state "myDevice", 0

Query Syntax

SYSTem:CONFigure:EDEVice:SMU:CHANnel[1-4]:STATe? <name>

Return Type

Boolean

Default

OFF


SYSTem:CONFigure:EDEVice:STATe <name>,<state>

Applicable Models: All

(Read-Write)  Set and return the state of activation of the device. When SYST:CONF:EDEV:IOEN = ON, and this command is set to ON, the VNA will attempt communication with the external device.

Send this command AFTER sending other external device settings (especially SYST:CONF:EDEV:DTYP) to avoid communicating with the device before it has been fully configured.

See Also: SYST:PREF:ITEM:EDEV:DPOL - Determines whether external devices remain activated or are de-activated when the VNA is Preset or when a Instrument State is recalled.

Parameters

 

<name>

String - Name of the device.

<state>

Boolean - Choose from:

OFF or 0 - Device is NOT activated

ON or 1 - Device is activated.

Examples

SYST:CONF:EDEV:STAT "myDevice", ON

system:configure:edevice:state "myDevice", 0

Query Syntax

SYSTem:CONFigure:EDEVice:STATe? <name>

Return Type

Boolean

Default

OFF - When configured using the front panel user interface, the device is ON (activated) by default.


SYSTem:CONFigure:EDEVice:TOUT <name>,<value>

Applicable Models: All

(Read-Write) Set and return the time out value for the specified external device. This is the time allowed for communication with the device before an error is generated.

Parameters

 

<name>

String - Name of the device.

<value>

Time out value in seconds.

Examples

SYST:CONF:EDEV:TOUT "myDevice",2

system:configure:edevice:tout "myDevice",5

Query Syntax

SYSTem:CONFigure:EDEVice:TOUT? <name>

Return Type

Numeric

Default

20


SYSTem:CONFigure:EDEVice:SOURce:DPPoint <name>,<value>

Applicable Models: All

(Read-Write) Sets and returns the amount of time the VNA should wait after for an external source to settle before making a measurement at each data point. This setting applies to all channels that use this external source.

Parameters

 

<name>

String - Name of the device.

<value>

Dwell time in seconds.

Examples

SYST:CONF:EDEV:SOUR:DPP "myDevice",2

system:configure:edevice:source:dppoint "myDevice",.1

Query Syntax

SYSTem:CONFigure:EDEVice:SOURce:DPP? <name>

Return Type

Numeric

Default

3.114 e-3


SYSTem:CONFigure:EDEVice:SOURce:HYBRid:INPut:FREQuency:CARRier <name>,<value>

Applicable Models: All

(Read-Write) For an SSB Mixer, the center of the input modulated signal is offset from DC by the carrier frequency.

The Hybrid Source will adjust the LO Source to set the frequency of the output. In some cases, the Input Carrier frequency must be adjusted by a slight amount so that the input mixed with the LO results in the desired output. This entry is labeled as being "Nominal" because the value may be changed by the Hybrid Source.

Parameters

 

<name>

String - Name of the device.

<value>

Carrier in Hz. Range is 0 to 10 GHz.

Examples

SYST:CONF:EDEV:SOUR:HYBRid:INPut:FREQuency:CARRier "myDevice",1e9

Query Syntax

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:INPut:FREQuency:CARRier? <name>

Return Type

Numeric

Default

0 Hz


SYSTem:CONFigure:EDEVice:SOURce:HYBRid:INPut:FREQuency:MULTiplier <name>,<value>

Applicable Models: All

(Read-Write) If there is a multiplier placed between the Input Source and the SSB mixer, then use this command to specify the multiplication factor.

Parameters

 

<name>

String - Name of the device.

<value>

Muliplier. Range is 1 to 999.

Examples

SYST:CONF:EDEV:SOUR:HYBR:INP:FREQ:MULT "myDevice",10

Query Syntax

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:INPut:FREQuency:MULTiplier? <name>

Return Type

Numeric

Default

1


SYSTem:CONFigure:EDEVice:SOURce:HYBRid:INPut:NAME <name>,<value>

Applicable Models: All

(Read-Write) Select external or internal sources for the input source.

Parameters

 

<name>

String - Name of the device.

<value>

String - Name of the input source.

Examples

SYST:CONF:EDEV:SOUR:HYBR:INP:NAME "myDevice","Port1"

Query Syntax

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:INPut:NAME? <name>

Return Type

String

Default

None


SYSTem:CONFigure:EDEVice:SOURce:HYBRid:INPut:POWer:LIMit <name>,<value>

Applicable Models: All

(Read-Write) This is the maximum power setting allowed for the Input Source.

The system will adjust the output power of the Hybrid Source by changing the power level of the Input Source and correcting for the Nominal Gain. This limit ensures that the Input Source is not set to a power level that will damage the SSB mixer.

Parameters

 

<name>

String - Name of the device.

<value>

Power Limit in dBm. Range is -200 to 100.

Examples

SYST:CONF:EDEV:SOUR:HYBR:INP:POW:LIM "myDevice",10

Query Syntax

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:INPut:POWer:LIMit? <name>

Return Type

Numeric

Default

0


SYSTem:CONFigure:EDEVice:SOURce:HYBRid:INPut:PULSe:ENABle <device>,<state>

Applicable Models: All

(Read-Write) Enables pulse on the Input Source.

The hybrid source can be pulsed either by pulsing the Input Source or by pulsing the LO Source. The user can choose which source is pulsed when the hybrid source is pulsed. See also, SCPI command description for enabling pulse on LO Source.

Parameters

 

<device>

String - Name of the device.

<state>

Boolean - Choose from:

OFF or 0 - Pulse  is NOT activated

ON or 1 - Pulse is activated.

Examples

SYST:CONF:EDEV:SOUR:HYBR:INP:PULS:ENAB "myDevice",1

Query Syntax

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:INPut:PULSe:ENABle? <device>

Return Type

Numeric

Default

0


SYSTem:CONFigure:EDEVice:SOURce:HYBRid:LO:FREQuency:MULTiplier <name>,<value>

Applicable Models: All

(Read-Write) If there is a multiplier placed between the LO Source and the SSB mixer, then use this command to specify the multiplication factor.

Parameters

 

<name>

String - Name of the device.

<value>

Muliplier. Range is 1 to 999.

Examples

SYST:CONF:EDEV:SOUR:HYBR:LO:FREQ:MULT "myDevice",10

Query Syntax

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:LO:FREQuency:MULTiplier? <name>

Return Type

Numeric

Default

1


SYSTem:CONFigure:EDEVice:SOURce:HYBRid:LO:NAME <name>,<value>

Applicable Models: All

(Read-Write) Select external or internal sources for the LO source.

Parameters

 

<name>

String - Name of the device.

<value>

String - Name of the LO source.

Examples

SYST:CONF:EDEV:SOUR:HYBR:LO:NAME "myDevice","Port1"

Query Syntax

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:LO:NAME? <name>

Return Type

String

Default

None


SYSTem:CONFigure:EDEVice:SOURce:HYBRid:LO:POWer <name>,<value>

Applicable Models: All

(Read-Write) Sets and returns the amount of time the VNA should wait after for an external source to settle before making a measurement at each data point. This setting applies to all channels that use this external source.

Parameters

 

<name>

String - Name of the device.

<value>

LO Power in dBm. Range is -200 to 100.

Examples

SYST:CONF:EDEV:SOUR:HYBR:LO:POW "myDevice",10

Query Syntax

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:LO:POWer? <name>

Return Type

Numeric

Default

0


SYSTem:CONFigure:EDEVice:SOURce:HYBRid:LO:PULSe:ENABle <device>,<state>

Applicable Models: All

(Read-Write) Enables pulse on the LO Source.

The hybrid source can be pulsed either by pulsing the Input Source or by pulsing the LO Source. The user can choose which source is pulsed when the hybrid source is pulsed. See also, SCPI command description for enabling pulse on Input Source.

Parameters

 

<device>

String - Name of the device.

<state>

Boolean - Choose from:

OFF or 0 - Pulse  is NOT activated

ON or 1 - Pulse is activated.

Examples

SYST:CONF:EDEV:SOUR:HYBR:LO:PULS:ENAB "myDevice",1

Query Syntax

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:LO:PULSe:ENABle? <device>

Return Type

Numeric

Default

0


SYSTem:CONFigure:EDEVice:SOURce:HYBRid:LOCK:STATe <device>,<state>

Applicable Models: All

(Read-Write) This locks out sources that are used by the hybrid source from the GUI. By default this is checked.

Parameters

 

<device>

String - Name of the device.

<state>

Boolean - Choose from:

OFF or 0 - Lock is NOT activated

ON or 1 - Lock is activated.

Examples

SYST:CONF:EDEV:SOUR:HYBR:LOCK:STAT "myDevice",0

Query Syntax

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:LOCK:STAT? <device>

Return Type

Numeric

Default

1


SYSTem:CONFigure:EDEVice:SOURce:HYBRid:OUTPut:FREQuency:MAX <device>,<value>

Applicable Models: All

(Read-Write) Sets the maximum output frequency limit of the mixer.

Parameters

 

<device>

String - Name of the device.

<value>

Maximum frequency limit for the mixer in Hz. Range is 0 to 1000 GHz.

Examples

SYST:CONF:EDEV:SOUR:HYBR:OUTP:FREQ:MAX "myDevice",10e9

Query Syntax

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:OUTP:FREQ:MAX? <device>

Return Type

Numeric

Default

1000 GHz


SYSTem:CONFigure:EDEVice:SOURce:HYBRid:OUTPut:FREQuency:MIN <device>,<value>

Applicable Models: All

(Read-Write) Sets the minimum output frequency limit of the mixer.

Parameters

 

<device>

String - Name of the device.

<value>

Minimum frequency limit for the mixer in Hz. Range is 0 to 1000 GHz.

Examples

SYST:CONF:EDEV:SOUR:HYBR:OUTP:FREQ:MIN "myDevice",10e6

Query Syntax

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:OUTP:FREQ:MIN? <device>

Return Type

Numeric

Default

0 Hz


SYSTem:CONFigure:EDEVice:SOURce:HYBRid:OUTPut:GAIN <device>,<value>

Applicable Models: All

(Read-Write) This is the nominal gain of the SSB mixer system. The nominal gain value is used to set the input source power in order to get the desired output source power. The user may choose to add an amplifier to the hybrid source to get more output power.

Note that if the input multiplier is set to some value other than 1, then the concept of amplification not very clear. In this case, we will assume that the gain represents the gain from the input power limit value to the resulting output power.

Parameters

 

<device>

String - Name of the device.

<value>

Gain in dB. Range is -200 to 100

Examples

SYST:CONF:EDEV:SOUR:HYBR:OUTP:GAIN "myDevice",10

Query Syntax

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:OUTPut:GAIN? <device>

Return Type

Numeric

Default

0 dB


SYSTem:CONFigure:EDEVice:SOURce:HYBRid:OUTPut:MIXer:SIDeband <device>,<value>

Applicable Models: All

(Read-Write) Specify whether to select the sum (High) or difference (Low) products. Input + or - LO = Output frequency

Parameters

 

<device>

String - Name of the device.

<value>

Sideband value. Choose from

LOW - Low or Difference (-)

HIGH - High or Sum (+)

Examples

SYST:CONF:EDEV:SOUR:HYBR:OUTP:MIX:SID "myDevice",HIGH

Query Syntax

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:OUTP:MIX:SID? <device>

Return Type

Character

Default

LOW


SYSTem:CONFigure:EDEVice:SOURce:HYBRid:TYPE <name>,<value>

Applicable Models: All

(Read-Write) Currently provides two selections: SSB Mixer (default) and Multiplier. The External Device dialog changes appearance and available settings according to the Hybrid Type you select.

Parameters

 

<name>

String - Name of the device.

<value>

String - Name of the Hybrid Type.

Examples

SYST:CONF:EDEV:SOUR:HYBR:TYPE "myDevice","Multiplier"

Query Syntax

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:TYPE? <name>

Return Type

String

Default

SSB Mixer


SYSTem:CONFigure:EDEVice:SOURce:MODulation:CONTrol:STATe <name>,<state>

Applicable Models: All

(Read-Write) Sets and reads the state of the modulation control. Modulation control must be ON to control the modulation of an external source.

Parameters

 

<name>

String - Name of the device.

<state>

ON (or 1)  Enable control of external modulation.

OFF (or 0)  Disable control of external modulation.

Learn about these settings and about adding an external source.

Examples

SYST:CONF:EDEV:SOUR:MOD:CONT:STAT "qasmxg",1

system:configure:edevice:source:modulation:control:state "qasmxg",OFF

Query Syntax

SYSTem:CONFigure:EDEVice:SOURce:MODulation:CONTrol:STATe? "qasmxg"

Default

OFF


SYSTem:CONFigure:EDEVice:SOURce:TMODe <name>,<value>

Applicable Models: All

(Read-Write) Sets and returns the trigger mode for an external source. Learn more.

Parameters

 

<name>

String - Name of the device.

<value>

Trigger Mode. Choose from:

CW - Software CW mode

HW - Hardware list mode

Examples

SYST:CONF:EDEV:SOUR:TMOD "myDevice",CW

system:configure:edevice:source:tmode "myDevice",hw

Query Syntax

SYSTem:CONFigure:EDEVice:SOURce:TMODe? "myDevice"

Return Type

Numeric

Default

Depends on Source and VNA Model


SYSTem:CONFigure:EDEVice:SOURce:TPORt <name>,<value>

Applicable Models: All

(Read-Write) Sets and returns the VNA port through which an external source is to be triggered.

Parameters

 

<name>

String - Name of the device.

<value>

Trigger Port. Choose from aux1 or aux2

Examples

system:configure:edevice:source:tport "myDevice",aux1

Query Syntax

SYSTem:CONFigure:EDEVice:SOURce:TPORt? <name>

Return Type

Character

Default

aux1