The following SCPI example demonstrates how to create a Narrowband Pulse Profile measurement using the Pulsed Application DLL on the PNA-X.
It first gets valid configuration settings and then uses those settings to configure the VNA and internal pulsed generators.
To run this program, you need:
PNA-X
Pulsed Application (Option H08)
This VBScript (*.vbs) program can be run as a macro in the VNA. To do this, copy the following code into a text editor file such as Notepad and save it on the VNA hard drive as PulseProfile.vbs. Learn how to setup and run the macro.
Note: Because of the long length of some commands in this example, word wrapping may occur when copying. These lines require modification after pasting.
Install and register the pulsed .dll on your PC.
ConfigEnhancedNB2 method for sending and returning parameters to the .dll.
ConfigEnhancedNBIFAtten method for setting the receiver IF gain.
SCPI IF Configuration commands used in the program.
|
public partial class Form1 : Form { private object pna; private object scpi; private Type srvtype; private AgilentPNAPulsed.applicationClass pulseApp; public Form1() { InitializeComponent(); } private string sendScpiCommand(string scpitext) { object[] parameter = new object[1]; parameter[0] = scpitext; return (string)srvtype.InvokeMember("parse", BindingFlags.InvokeMethod, null, scpi, parameter); } private void ConnectToPNA() { srvtype = Type.GetTypeFromProgID("AgilentPNA835x.Application", true); pna = Activator.CreateInstance(srvtype); scpi = srvtype.InvokeMember("ScpiStringParser", BindingFlags.GetProperty, null, pna, null); } private void NBGPIBbutton_Click(object sender, EventArgs e) { double dPRF = 10000, dBW = 500; //PRF=10kHz double dPhysicalIF = 0, dNCO = 0, dClockFreq = 0; System.Array aStage1TapArray = null, aStage2TapArray = null, aStage3TapArray = null; bool bFixedPRF = true; double dGateDelay = 0.0, dGateWidth = 0.00000005; //Gate width=50ns double dSWGateDelay = 0, dSWGateWidth = 0; int iSWGateRamp = 0; double dModPulseWidth = 0.00001;//10 us double dModPulseDelay = 0.00001;//10us short myAtten = 0; pulseApp = new AgilentPNAPulsed.applicationClass(); ConnectToPNA(); //Preset PNA-X sendScpiCommand("*RST"); //Measure S21 sendScpiCommand("DISP:WIND:TRAC1:DEL"); sendScpiCommand("CALCulate:PARameter:DEFine:EXT /'MyMeas/',S21"); sendScpiCommand("DISP:WIND:TRAC1:FEED /'MyMeas/'"); //Set power leveling mode to Openloop sendScpiCommand("sour:pow1:alc:mode open"); //Send desired pulsed parameters to the pulsed configuration DLL. //The DLL will return a new set of pulse parameters to send to the PNA-X. pulseApp.ConfigEnhancedNB2(ref dPRF, ref dBW, ref dPhysicalIF, ref dNCO, ref dClockFreq, ref aStage1TapArray, ref aStage2TapArray, ref aStage3TapArray, bFixedPRF, dGateDelay, dGateWidth, ref dSWGateDelay, ref dSWGateWidth, ref iSWGateRamp);
double pulsePeriod = 1 / dPRF; //Pulse #1 as modulation source sendScpiCommand("sens:puls:per " + pulsePeriod.ToString()); // 100us //Set Pulse1 width sendScpiCommand("sens:puls1:width "+dModPulseWidth.ToString()); //10us //Set Pulse1 delay sendScpiCommand("sens:puls1:delay " + dModPulseDelay.ToString()); //10us //Turn on Pulse1 sendScpiCommand("SENS:PULS1:STAT 1"); //Set modulation source to Pulse1 sendScpiCommand("sens:path:conf:elem /"PulseModDrive/",/"Pulse1/""); //Enable pulse modulator 1 sendScpiCommand("sens:path:conf:elem /"Src1Out1PulseModEnable/",/"Enable/""); //Pulse #2 controls receiver gate sendScpiCommand("sens:puls2:width " + dGateWidth.ToString()); //50ns sendScpiCommand("sens:puls2:delay " + dGateDelay.ToString()); //0 sendScpiCommand("SENS:PULS2:STAT 1"); sendScpiCommand("sens:path:conf:elem /"IFGateA/",/"Pulse2/""); sendScpiCommand("sens:path:conf:elem /"IFGateB/",/"Pulse2/""); sendScpiCommand("sens:path:conf:elem /"IFGateR1/",/"Pulse2/""); sendScpiCommand("sens:path:conf:elem /"IFGateR2/",/"Pulse2/""); //Set IFBW sendScpiCommand("SENS:BWID "+dBW.ToString()); //Configure IF path sendScpiCommand("sens:path:conf:elem /"IFSigPathAll/",/"NBF/""); sendScpiCommand("SENS:IF:FILT:AUTO 0"); sendScpiCommand("SENS:IF:FREQ:AUTO 0"); sendScpiCommand("SENS:IF:FREQ "+dPhysicalIF.ToString()); // Set filter stages based on pulse parameters sendScpiCommand("SENS:IF:FILT:STAGe1:FREQ " + dNCO.ToString()); //Convert Stage1TapArray to string string buf1 = new string(' ', 1000); for (int i = 0; i < aStage1TapArray.GetLength(0); i++) { buf1 = buf1 + aStage1TapArray.GetValue(i).ToString()+","; } buf1 = buf1.Trim(); buf1 = buf1.Substring(0, buf1.Length - 1); //Convert Stage1TapArray to string string buf2 = new string(' ', 1000); for (int j = 0; j < aStage2TapArray.GetLength(0); j++) { buf2 = buf2 + aStage2TapArray.GetValue(j).ToString() + ","; } buf2 = buf2.Trim(); buf2 = buf2.Substring(0, buf2.Length - 1); //Set IF Filter Stage1 and Stage2 Coeficent sendScpiCommand("SENS:IF:FILT:STAG1:COEF " + buf1 ); sendScpiCommand("SENS:IF:FILT:STAG2:COEF " + buf2); if (dSWGateWidth == 0) // No valid SW gate { sendScpiCommand("SENS:IF:FILT:STAG3:TYPE 'RECT'"); sendScpiCommand("SENS:IF:FILT:STAGe3:PAR 'C'," + aStage3TapArray.GetValue(0).ToString()); sendScpiCommand("SENS:PULS0:STAT 0"); } else { sendScpiCommand("SENS:IF:FILT:STAGe3:TYPE 'PWIN'"); sendScpiCommand("SENS:IF:FILT:STAGe3:PAR 'C'," + aStage3TapArray.GetValue(0).ToString()); sendScpiCommand("SENS:IF:FILT:STAGe3:PAR 'P'," + pulsePeriod.ToString()); sendScpiCommand("SENS:IF:FILT:STAGe3:PAR 'D'," + dSWGateDelay.ToString()); sendScpiCommand("SENS:IF:FILT:STAGe3:PAR 'W'," + dSWGateWidth.ToString()); sendScpiCommand("SENS:IF:FILT:STAGe3:PAR 'R'," + iSWGateRamp.ToString()); double pulse0Width=1/dClockFreq; sendScpiCommand("sens:puls0:width " + pulse0Width.ToString()); sendScpiCommand("sens:puls0:delay 0"); sendScpiCommand("SENS:PULS0:STAT 1"); }
pulseApp.ConfigEnhancedNBIFAtten(dPRF, dGateWidth, ref myAtten); sendScpiCommand("sens:path:conf:elem /"NBFATNA/",/""+myAtten.ToString()+ "/""); sendScpiCommand("sens:path:conf:elem /"NBFATNB/",/"" + myAtten.ToString() + "/""); sendScpiCommand("sens:path:conf:elem /"NBFATNR1/",/"" + myAtten.ToString() + "/""); sendScpiCommand("sens:path:conf:elem /"NBFATNR2/",/"" + myAtten.ToString() + "/""); //Run pulse profile using below several lines //Set CW Mode sendScpiCommand("SENS:SWE:TYPE CW"); double startTime, stopTime, stepTime; int myProfilePoints; startTime = 0.00001;//10us stopTime = 0.00005;//50us stepTime = 0.00000005;//50ns myProfilePoints = (int)((stopTime - startTime) / stepTime) + 1; sendScpiCommand("SENS:SWE:POIN " + myProfilePoints.ToString()); // Test gates sendScpiCommand("sens:puls1:delay " + startTime.ToString()); sendScpiCommand("SENS:PULS2:DINC " + stepTime.ToString()); //Single Sweep sendScpiCommand("SENS:SWE:MODE SING"); sendScpiCommand("DISP:WIND:TRAC:Y:AUTO"); } } |