Basic Control using VEE


This VEE Pro 6.0 example does the following:

If this Help file is on a VNA and VEE Pro RunTime is installed, then:

  1. Run the BasicControl.vxe example

  2. Then click Open on the following dialog box to run the program.

Otherwise, you can modify the example program using VEE, save the VEE BasicControl.vee

Learn how to run this program as a Macro on the VNA.


The following dialog box will be visible on the VNA when the example program is running.