Beginning in Dec. 2005, Keysight VEE Pro RunTime is installed on new VNAs. This means that programs written with Keysight VEE (.vxe files) can be run directly on the VNA.
VNAs without Keysight VEE installed can go to the Keysight VEE website and download Keysight VEE Pro 6.2 RunTime to the VNA and begin to run VEE programs directly on the VNA. This version does not require Keysight I/O Libraries suite 14. Do NOT upgrade to Keysight I/O libraries suite 14 on the VNA.
With Keysight VEE Pro RunTime installed on the VNA, the following examples can be run directly on the VNA:
Basic Control of the VNA
For more VEE examples, see the PNA support website.
For more information on Keysight VEE, see www.Keysight.com/find/VEE